This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMK1D1208:有关 LMK1D1208的问题

Guru**** 2925550 points

Other Parts Discussed in Thread: LMK1D1208, LMK1D1208P, LMK1D1208I

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1105556/lmk1d1208-question-about-lmk1d1208

器件型号:LMK1D1208

尊敬的 TI:

问题1.

LMK1d1208的数据表写入输入50%占空比时钟、输出占空比为45%至55%。 如果输入时钟占空比为2%(200kHz)、那么输出占空比是多少?

问题2.

LMK1d1208是否可用作 LVDS 数据传输?

问题3.

输入信号是占空比为0.2%至0.6%的200kHz LVDS 信号、可输出相同 LVDS 信号的6个以上通道。 温度范围为-40至105度。 最好每个通道都具有单独的使能信号。 您能否推荐满足上述要求的芯片?