请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:CDCI6214您好、社区
请根据以下规格推荐时钟合成器部件:
电源内核电压(VDDA、VDDD、VDDO):1.8V
输入数:1 (晶振输入25MHz)
输出数量:2.
所需输出频率:156.25MHZ
可通过:I2C 接口进行编程
封装:16-LGA
谢谢、此致、
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.