我想确认 LMX2572LP 的 OSCin (单端输入缓冲器)的输入电平。
在目录中、OSCin 输入电压列为最小值:0.3到最大值:3.6V。
假设这个值是图154中的 Vp-p 是安全的吗?
如果阻抗为50Ω、是否可以安全地假设 Min:-6.48dBm 至 max:15.11dBm?
此致、
横内明彦
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 Yokouchi-San:
正确、如果您使 IPBUF_TERM = 1、则不需要 R25。 在单端输入模式下、IPBUF_TYPE = 1、OSCin*引脚被忽略、因此我们可以保持 R30。
例如、如果50Ω 源为1V、则 OSCIN 引脚处的电压为1V:
- IPBUF_TERM = 1、R25被删除
- IPBUF_TERM = 0、R25已填充