This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PLLATINUMSIM-SW:PLLatinum SIM 软件未处理的异常

Guru**** 2589275 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1348123/pllatinumsim-sw-pllatinum-sim-software-unhandled-exception

器件型号:PLLATINUMSIM-SW

您好

我在运行 PLLatinum Sim 软件(版本1.6.5)时遇到问题。 我在启动软件时一直收到以下异常。 我有 Microsoft。 安装在 Windows 11上的 NET 4.8。

我已尝试在另一台计算机上安装此软件、但收到相同的错误。

您可以提供帮助吗?

 

See the end of this message for details on invoking 
just-in-time (JIT) debugging instead of this dialog box.

************** Exception Text **************
System.InvalidCastException: Conversion from string "1.365" to type 'Double' is not valid. ---> System.FormatException: Input string was not in a correct format.
   at Microsoft.VisualBasic.CompilerServices.Conversions.ParseDouble(String Value, NumberFormatInfo NumberFormat)
   at Microsoft.VisualBasic.CompilerServices.Conversions.ToDouble(String Value, NumberFormatInfo NumberFormat)
   --- End of inner exception stack trace ---
   at Microsoft.VisualBasic.CompilerServices.Conversions.ToDouble(String Value, NumberFormatInfo NumberFormat)
   at Microsoft.VisualBasic.CompilerServices.Conversions.ToDouble(String Value)
   at TIPLLatinumSim.TIPLLatinumForm.SearchDevices()
   at TIPLLatinumSim.TIPLLatinumForm.cmb_SD_DeviceType_SelectedIndexChanged(Object sender, EventArgs e)
   at System.Windows.Forms.ComboBox.OnSelectedIndexChanged(EventArgs e)
   at System.Windows.Forms.ComboBox.set_SelectedIndex(Int32 value)
   at TIPLLatinumSim.TIPLLatinumForm.FilterDesignerForm_Load(Object sender, EventArgs e)
   at System.EventHandler.Invoke(Object sender, EventArgs e)
   at System.Windows.Forms.Form.OnLoad(EventArgs e)
   at System.Windows.Forms.Form.OnCreateControl()
   at System.Windows.Forms.Control.CreateControl(Boolean fIgnoreVisible)
   at System.Windows.Forms.Control.CreateControl()
   at System.Windows.Forms.Control.WmShowWindow(Message& m)
   at System.Windows.Forms.Control.WndProc(Message& m)
   at System.Windows.Forms.ScrollableControl.WndProc(Message& m)
   at System.Windows.Forms.ContainerControl.WndProc(Message& m)
   at System.Windows.Forms.Form.WmShowWindow(Message& m)
   at System.Windows.Forms.Form.WndProc(Message& m)
   at System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
   at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
   at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)


************** Loaded Assemblies **************
mscorlib
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9181.0 built by: NET481REL1LAST_C
    CodeBase: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
----------------------------------------
TIPLLatinumSim
    Assembly Version: 1.6.5.0
    Win32 Version: 1.6.5.0
    CodeBase: file:///C:/Program%20Files%20(x86)/Texas%20Instruments/PLLatinumSim/TIPLLatinumSim.exe
----------------------------------------
Microsoft.VisualBasic
    Assembly Version: 10.0.0.0
    Win32 Version: 14.8.9032.0 built by: NET481REL1
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Microsoft.VisualBasic/v4.0_10.0.0.0__b03f5f7f11d50a3a/Microsoft.VisualBasic.dll
----------------------------------------
System.Windows.Forms
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9181.0 built by: NET481REL1LAST_C
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9220.0 built by: NET481REL1LAST_C
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9032.0 built by: NET481REL1
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
System.Configuration
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9032.0 built by: NET481REL1
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
----------------------------------------
System.Core
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9220.0 built by: NET481REL1LAST_C
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
System.Xml
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9032.0 built by: NET481REL1
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
Accessibility
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9032.0 built by: NET481REL1
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
----------------------------------------
System.Runtime.Remoting
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9214.0 built by: NET481REL1LAST_B
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Runtime.Remoting/v4.0_4.0.0.0__b77a5c561934e089/System.Runtime.Remoting.dll
----------------------------------------
System.Windows.Forms.DataVisualization
    Assembly Version: 4.0.0.0
    Win32 Version: 4.8.9032.0
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms.DataVisualization/v4.0_4.0.0.0__31bf3856ad364e35/System.Windows.Forms.DataVisualization.dll
----------------------------------------

************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.

For example:

<configuration>
    <system.windows.forms jitDebugging="true" />
</configuration>

When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.


谢谢

R·西布里特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是一个定位问题、其中 PLLatinum Sim 尝试 解析不变培养中保存的初始化值、而是解析系统局部培养中的值。 我会通知维护人员、在接下来的几天里、将会有一个修复程序在 v1.6.6.0中提供。  现在,作为一种解决方法,您可以将 系统编号格式设置为使用 en-US 语言环境:

    • 控制面板 -> 时钟和区域 -> 在"区域"下、选择 更改日期、时间或数字格式 ->  其他设置... -> 设置  十进制符号:  更改为"。" 和  数字分组符号: 更改为"、"
    •   使用 PLLatinum Sim 完成后、您可以使用"复位"按钮复位这些设置。

    对于给您带来的不便、我们深表歉意。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 Derek、这解决了我的问题。