This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS:Windows 7 x64上的7.0 .0.0.0042万 (带Eclipse 4.6):调试视图中的"未处理循环异常"

Guru**** 2538930 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/565751/ccs-ccs7-0-0-00042-with-eclipse-4-6-on-windows-7-x64-unhandled-loop-exception-in-debug-view

工具/软件:Code Composer Studio

您好,

我一直在玩CCS v7,切换到CCS调试视图并激活表达式窗口后,立即遇到非致命异常:

来自.log的片段:

!stack 0
org.eclipse.swt.swt错误: 小
	
	
	
	
	
	org.eclipse.swt.widgets.Composite.createHandle(Composite.java:315
	
	
	
	部件位于org.eclipse.swt.swt.error(SWT.java:4559) at org.eclipse.swt.swt.error(Swt.java:4448)小部件位于org.eclipse.swt.swt.crle.scle:swimet.scle:swa.scle.scle.screp.scle:se.script.toolbar.swabet.swabet.swa.se.swa.scle:se.screips.scle:swa.se.scrips.scr.screatewa.scle:swa.scr.screatewa.scle:swa.scr.toolbar.scr.swa.ips.ga.ips.ga.scle:swa.ips.ga.ips.ga.ips.ga.ips.gabet.toolbars.ga.se.ga.scle:swa.se.ga.se.ga.ips.ga.se.screabe.scr.swa.se.ga.scr.swa.scr.swa.
	
	
	org.eclipse.swt.widgets.Composite.<init>(Composite.java:96
	
	org.eclipse.swt.custom.CTabFolder.setButtonBounds(CTabFolder.java:2478
	
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84
	org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1084
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) at org.eclipse.swt.widgets.Control.wm_size(Control.java:5459) at org.eclipse.swt.scrollable.wm_size(scrollable.java:367) at org.eclipse.swt.widgets.Composite.WM_SIZE(Composite.java:1783
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88) at org.eclipse.swwm.swwme.swwindowt.windowproc.windowproc(Control.windowproc)at org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native at
	
	
	
	org.eclipse.swt.internal.win32.OS.SetWindowPos(Native at
	wme.eclipse.swt.widget.setWindowPoos (Widget.java:1482)
	org.eclipse.swt.widgets.Control.setBoundsInPixels(Control.java:3251
	
	
	org.eclipse.swt.widgets.Control.setSizeInPixels(Control.java:3776
	
	
	
	
	org.eclipse.debug.internal.ui.views.variables.VariablesView.setGlobalActions(VariablesView.java:705
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84
	
	
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103) org.eclipse.swt.widgets.Control.setBoundsInPixels(Control.java:3212) org.eclipse.swt.widgets.Composite.setBoundsInPixels(Composite.java:1099) org.eclipse.swt.swt.Control.pack (Control.java.wm:2175) wme.swwm_wme.gpetse.gipse.webs (swwme.gwme.gpetc.ecs.c.c.glipse.webnits.c.webs) org.eclipse.ui.internal.e4.compatibility.ActionBars.updateActionBars(ActionBars.java:83 (swwme.gwme.gpetse.gpetwme.gpetse.gpetse.webs org.eclipse.debug.internal.ui.views.variables.VariablesView4美元.focusGained(VariablesView.java:664) org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079)
	
	org.eclipse.swt.widgets.Control.sendFocusEvent(Control.java:2926 org.eclipse.swt.widgets.Control.setSize(Control.java:3806 org.eclipse.debug.internal.ui.views.variables.VariablesView.access3美元(VariablesView.java:696 org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1084)
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.SetFocus(Native Method)
	,网址为:org.eclipse.swt.widgets.Control.forceFocus (Control.java:1114)
	,网址
	为org.eclipse.swt.widgets.Composite.setFocus(Composite.java:1121,
	网址为org.eclipse.debug.internal.ui.views.variables.VariablesView.setFocus(VariablesView.java:1535
	,网址为org.eclipse.swt.widgets.Control.setFocus(Control.java:3439 org.eclipse.ui.internal.e4.compatibility.CompatibilityPart.delegateSetFocus(CompatibilityPart.java:204,
	网址为sun.reflect.GeneratedMethodAccessor83.invoke(Unknown Source)
	sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43
	
	) org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:54
	)
	
	org.eclipse.e4.core.internal.di.InjectorImpl.invoke(InjectorImpl.java:259)
	
	
	org.eclipse.e4.ui.internal.workbench.PartServiceImpl.activate(PartServiceImpl.java:751)
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)
	
	
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103
	
	
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)()))(windowPartRenderer.java:63)))))(org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:282)(org.eclipse.e4.core.contexts.ContextInjectionFactory.invoke(ContextInjectionFactory.java:107) wme.workworkworkworkworker.renders.swt.Contributers.ContributedPartRenderer1美元.handleEvents:windowPartn时至) wm:windowPartRenderers.java.mander.java:wm:wm:wm:wm:wm:windowPartRender.ava:() java.lang.reflect.Method.invoke(Method.java:498 org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:288 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.focusGui(PartRenderingEngine.java:779 org.eclipse.e4.ui.internal.workbench.swt.AbstractPartRenderer.activate(AbstractPartRenderer.java:95 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079 org.eclipse.swt.widgets.Shell.setActiveControl(Shell.java:1542) org.eclipse.e4.ui.internal.workbench.PartServiceImpl.activate(PartServiceImpl.java:682 () org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410) org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1088)())
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	(
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (Display.java:5115)
	
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547)
	
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)(org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547))()()()()网站上的SWlipse.swt.Control.proc(Display.java.)上的SWlips.windowproc(javecs.ge.gobet)())上的SWlipe.windowproecse.ge.gipe.gips.())()上的微件()
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547 org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547))) org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547),网址:org.eclipse.swt.widgets.Display.windowProc (Display.java:5115)),网址:() org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) at org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	) at org.eclipse.swt.widgets.Control.windowProc (Control.java:4889)
	at org.eclipse.swt.widgets.Display.windowProc (Display.java:5115)
	at org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547)
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native
	
	
	
	
	
	
	
	
	(org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native org.eclipse.swt.internal.win32.OS.CallWindowProcW(Native org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547上的微小部件:swese.windowprose.windowprose.java.ore.531.org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88 org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88 org.eclipse.swt.widgets.Tree.callWindowProc(Tree.java:1460)
	org.eclipse.swt.internal.win32.OS.CallWindowProc(OS.java:2446
	),网址为org.eclipse.swt.widgets.Tree.callWindowProc(Tree.java:1552
	
	
	
	
	
	
	org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine4美元.run(PartRenderingEngine.java:1121
	
	
	org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:150
	
	
	org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:604
	
	
	
	org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134
	
	
	org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243),网址为org.eclipse.swt.widgets.Control.windowProc (Control.java:4889),网址为org.eclipse.swt.internal.win32.OS.PeekMessageW(Native org.eclipse.swt.internal.win32.OS.PeekMessage(OS.java:3144 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1022 org.eclipse.ui.internal.Workbench5美元.run(Workbench.java:687 org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:138 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104
	sun.reflect.NativeMethodAccessorImpl.invoke0(Native org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336 org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388
	sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62
	
	),网址为java.lang.reflect.Method.invoke(Method.java:498
	),网址为org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:673)
	,网址为org.eclipse.equinox.launcher.Main.basicRun(Main.java:610)
	,网址为sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43 org.eclipse.equinox.launcher.Main.run(Main.java:1519)。 

如果我创建Eclipse CDT项目,然后切换到调试视图(创建远程调试配置),则CCS会出现相同的错误。

!entry org.eclipse.ui 4 0 2017年01月06日 21:54: 10.951
!message unhandled event loop exception
!stack 0
org.eclipse.swt.swtError: 小
	
	
	
	
	
	org.eclipse.swt.widgets.Composite.createHandle(Composite.java:315
	
	
	
	部件位于org.eclipse.swt.swt.error(SWT.java:4559) at org.eclipse.swt.swt.error(Swt.java:4448)小部件位于org.eclipse.swt.swt.crle.scle:swimet.scle:swa.scle.scle.screp.scle:se.script.toolbar.swabet.swabet.swa.se.swa.scle:se.screips.scle:swa.se.scrips.scr.screatewa.scle:swa.scr.screatewa.scle:swa.scr.toolbar.scr.swa.ips.ga.ips.ga.scle:swa.ips.ga.ips.ga.ips.ga.ips.gabet.toolbars.ga.se.ga.scle:swa.se.ga.se.ga.ips.ga.se.screabe.scr.swa.se.ga.scr.swa.scr.swa.
	
	
	org.eclipse.swt.widgets.Composite.<init>(Composite.java:96
	
	org.eclipse.swt.custom.CTabFolder.setButtonBounds(CTabFolder.java:2478
	
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84
	org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1084
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) at org.eclipse.swt.widgets.Control.wm_size(Control.java:5459) at org.eclipse.swt.scrollable.wm_size(scrollable.java:367) at org.eclipse.swt.widgets.Composite.WM_SIZE(Composite.java:1783
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88) at org.eclipse.swwm.swwme.swwindowt.windowproc.windowproc(Control.windowproc)at org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native at
	
	
	
	org.eclipse.swt.internal.win32.OS.SetWindowPos(Native at
	wme.eclipse.swt.widget.setWindowPoos (Widget.java:1482)
	org.eclipse.swt.widgets.Control.setBoundsInPixels(Control.java:3251
	
	
	org.eclipse.swt.widgets.Control.setSizeInPixels(Control.java:3776
	
	
	
	
	org.eclipse.debug.internal.ui.views.variables.VariablesView.setGlobalActions(VariablesView.java:705
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84
	
	
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103) org.eclipse.swt.widgets.Control.setBoundsInPixels(Control.java:3212) org.eclipse.swt.widgets.Composite.setBoundsInPixels(Composite.java:1099) org.eclipse.swt.swt.Control.pack (Control.java.wm:2175) wme.swwm_wme.gpetse.gipse.webs (swwme.gwme.gpetc.ecs.c.c.glipse.webnits.c.webs) org.eclipse.ui.internal.e4.compatibility.ActionBars.updateActionBars(ActionBars.java:83 (swwme.gwme.gpetse.gpetwme.gpetse.gpetse.webs org.eclipse.debug.internal.ui.views.variables.VariablesView4美元.focusGained(VariablesView.java:664) org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079)
	
	org.eclipse.swt.widgets.Control.sendFocusEvent(Control.java:2926 org.eclipse.swt.widgets.Control.setSize(Control.java:3806 org.eclipse.debug.internal.ui.views.variables.VariablesView.access3美元(VariablesView.java:696 org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1084)
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.SetFocus(Native Method)
	,网址为:org.eclipse.swt.widgets.Control.forceFocus (Control.java:1114)
	,网址
	为org.eclipse.swt.widgets.Composite.setFocus(Composite.java:1121,
	网址为org.eclipse.debug.internal.ui.views.variables.VariablesView.setFocus(VariablesView.java:1535
	,网址为org.eclipse.swt.widgets.Control.setFocus(Control.java:3439 org.eclipse.ui.internal.e4.compatibility.CompatibilityPart.delegateSetFocus(CompatibilityPart.java:204,
	网址为sun.reflect.GeneratedMethodAccessor74.invoke(Unknown Source)
	sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43
	
	) org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:54
	)
	
	org.eclipse.e4.core.internal.di.InjectorImpl.invoke(InjectorImpl.java:259)
	
	
	org.eclipse.e4.ui.internal.workbench.PartServiceImpl.activate(PartServiceImpl.java:751)
	
	
	
	org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)
	
	
	org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1103
	
	
	
	
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)()))(windowPartRenderer.java:63)))))(org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:282)(org.eclipse.e4.core.contexts.ContextInjectionFactory.invoke(ContextInjectionFactory.java:107) wme.workworkworkworkworker.renders.swt.Contributers.ContributedPartRenderer1美元.handleEvents:windowPartn时至) wm:windowPartRenderers.java.mander.java:wm:wm:wm:wm:wm:windowPartRender.ava:() java.lang.reflect.Method.invoke(Method.java:498 org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:288 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.focusGui(PartRenderingEngine.java:779 org.eclipse.e4.ui.internal.workbench.swt.AbstractPartRenderer.activate(AbstractPartRenderer.java:95 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1079 org.eclipse.swt.widgets.Shell.setActiveControl(Shell.java:1542) org.eclipse.e4.ui.internal.workbench.PartServiceImpl.activate(PartServiceImpl.java:682 () org.eclipse.swt.widgets.Display.sendEvent(Display.java:4410) org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1088)())
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	(
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (Display.java:5115)
	
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547)
	
	org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)(org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547))()()()()网站上的SWlipse.swt.Control.proc(Display.java.)上的SWlips.windowproc(javecs.ge.gobet)())上的SWlipe.windowproecse.ge.gipe.gips.())()上的微件()
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native)
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547 org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547) org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native (org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547))) org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547),网址:org.eclipse.swt.widgets.Display.windowProc (Display.java:5115)),网址:() org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) at org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88
	) at org.eclipse.swt.widgets.Control.windowProc (Control.java:4889)
	at org.eclipse.swt.widgets.Display.windowProc (Display.java:5115)
	at org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native
	org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547)
	
	
	
	org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native
	
	
	
	
	
	
	
	
	(org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547
	) org.eclipse.swt.internal.win32.OS.DefWindowProcW(Native org.eclipse.swt.internal.win32.OS.CallWindowProcW(Native org.eclipse.swt.internal.win32.OS.DefWindowProc(OS.java:2547上的微小部件:swese.windowprose.windowprose.java.ore.531.org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88 org.eclipse.swt.widgets.Scrollable.callWindowProc(Scrollable.java:88 org.eclipse.swt.widgets.Tree.callWindowProc(Tree.java:1460)
	org.eclipse.swt.internal.win32.OS.CallWindowProc(OS.java:2446
	),网址为org.eclipse.swt.widgets.Tree.callWindowProc(Tree.java:1552
	
	
	
	
	
	
	org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine4美元.run(PartRenderingEngine.java:1121
	
	
	org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:150
	
	
	org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:604
	
	
	
	org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134
	
	
	org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243),网址为org.eclipse.swt.widgets.Control.windowProc (Control.java:4889),网址为org.eclipse.swt.internal.win32.OS.PeekMessageW(Native org.eclipse.swt.internal.win32.OS.PeekMessage(OS.java:3144 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1022 org.eclipse.ui.internal.Workbench5美元.run(Workbench.java:687 org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:138 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104
	sun.reflect.NativeMethodAccessorImpl.invoke0(Native org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336 org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388
	sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62
	),
	位于java.lang.reflect.Method.invoke(Method.java:498
	),位于org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:673
	),位于org.eclipse.equinox.launcher.Main.basicRun(Main.java:610)
	,位于sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43 org.eclipse.equinox.launcher.Main.run(Main.java:1519

!entry org.eclipse.core.jobs 2 2017年01月06日 21:54: 20.390
!消息Job found still running after platform shutdown。 在关闭期间安排作业的插件应取消作业:COM.TI.CCStudio.leru.model.FilteredItemsSelectionDialog$FilterJob 

CCS安装在C:\ti\ccsv7中

可以忽略该错误:我单击"确定",而不是退出工作台。 但是,错误本身非常烦人,每次切换到表达式视图时都会弹出。 

请告诉我您的建议。

谢谢!

亚历山大

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Alexander,

    我对延迟回复表示歉意。 工程团队分析了您的日志并进行了以下分析:

    "错误消息可能不是特定于表达式视图的。 一旦处于此状态,打开其他视图可能会触发类似的错误(即无SWT句柄)。 当视图请求进程已用尽的资源(例如图形资源,但不限于此资源)时,将触发此错误。 这很可能是这些资源泄漏的症状。 再现这种情况将很棘手,因为客户可能已经使用CCS多日,而没有关闭CCS以耗尽资源…。 或者,它可能是另一个经常打开/重新打开的视图,以触发此耗尽。 它可能有助于收集一些有关客户工作流的信息,以查看是否有任何序列会快速触发此问题。 "

    他建议在出现这类问题时重新启动CCS。

    希望这有所帮助

    KI

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    由于某种原因,此问题在一台计算机上一直存在(打开“CCS调试”视图后100 % 可重现),而在另一台计算机上根本不会发生。

    我不知道有什么不同。  两个运行Windows 7 x64的版本相同。 失败的CCS安装在 C:\ti\ccsv7中,工作的CCS安装在 C:\ti\ccs700中。  这是否是根本原因?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    失败的CCS安装在 C:\ti\ccsv7中,工作的CCS安装在 C:\ti\ccs700中。  这是否是根本原因?[/QUOT]

    不,这不是问题。 这些路径看起来非常好

    对于出现故障的安装,您是否尝试使用了新的工作区文件夹?

    谢谢

    KI