工具/软件:Code Composer Studio
您好,
我们正在通过命令行创建一个'emptyAssemblyOnly"项目,该项目具有6个生成配置。 在夜间构建测试自动化过程中,我们需要使用遇到问题的shell脚本逐个构建每个构建配置。
我们发现,生成配置被切换为错误的配置,而不是使用-CCS.configuration参数指定的配置。 我在脚本中放置了回显消息,只是为了确保从父脚本正确传递$build_config_name变量值。
以下是脚本命令和示例输出供参考:
回应"正在为$build_config_name构建配置构建项目${project_name ..."
$CCS_INSTALL_DIR/eclipse/eclipse -noSplash -data "$CCS_Workspace_LOC"-application com.ti.ccstudio.apps.projectBuild -ccs.projects $project_name -CCS.configuration $build_config_name -CCS.buildType full
正在为PRU1_IRT构建配置构建项目Profinet交换机...[在shell脚本中添加回显消息]
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
CCS无外设构建正在启动... [星期二2月21日16:50:17 IST 2017 ]
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
=============================================================================================================
预处理...
=============================================================================================================
正在构建...
****为项目Profinet交换机构建配置PRU0_IRT ****[生成时显示消息]
我们发现此行为完全是随机的,并在不同的时间发生在不同的构建配置中。 是否有任何线索可以说明为什么生成配置与指定配置不符。 要跟踪此问题,需要进一步检查哪些要点?
此致,
Nijin P