This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/TMS320F2.8069万M:Code Composer Studio的MATLAB/Simulink支持

Guru**** 2538955 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/579389/ccs-tms320f28069m-matlab-simulink-support-for-code-composer-studio

部件号:TMS320F2.8069万M

工具/软件:Code Composer Studio

是否有某种来源可以找到有关MATLAB/Simulink的哪些特定版本与特定版本的Code Composer Studio兼容的最新信息? 具体来说,我需要知道CCSv7是否与R2016a兼容,如果不再兼容,最好知道是否有其他选项可用。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,Aleksander:

    R2016a中不支持CCSv7。 事实上,CCWorks R2016a在7.0 2016年12月发布,之后是2016年3月发布的。

    我知道开发团队正在积极努力添加CCSv7支持,但我不知道何时完成。

    我认为您可以使用CCSv7导入MathWorks产品生成的代码,但我尚未尝试。 C2000支持软件包仍然只能与CCSv6 (F2837x和F2807x需要)配合使用。

    一些信息见 :processors.wiki.ti.com/.../MatLab_and_CCS

    HTH,
    -Brian