This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS:CCSSEGV. 6.1 3.0.0034万 安装失败,并出现重复的"runEclipseApp -错误代码:CHILDKILLED 1.5671万 SIGSEGV {segmentation violation}"

Guru**** 2584215 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/606212/ccs-ccs6-1-3-00034-install-fails-with-repeated-runeclipseapp---errorcode-childkilled-15671-sigsegv-segmentation-violation

工具/软件:Code Composer Studio

您好,

我正在尝试按照 http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK上的说明构建处理器SDK

machine="am57xx-evi" bitbake tisdk-rootfs-image 

我得到以下结果(在完成某些步骤后):

错误:TI-ccsv6-native-esk.tmp-external-linaro-toolchain/work 6.1 /x86_64-linux/ti-ccsv6-native:LIC_files_CHKSUM指向无效文件:/tisdk/build/arago-tmp-external-linaroaro-toolchain/work /x86_64-linux/ti-ccsv6-native.ccsv6/native 6.1 3.0.0034万
-faretsfar-r0/ccss-ccvfulfar/doc-ccvfar-ccvfar-r/securr/securr/securr/securr/securr/securr/secure- 3.0.0034万 3.0.0034万 EULA.doc 6.1
错误:TI-ccsv6-native-toolchain/work 6.1
/x86_64-linux/ti-cc6-native/ccti.ctv-r0/temp/log.do_tmp-external-linaro-toolchain/work /x86_64-cc6-native/cctis.cm-r/temp/log.do_configure/native
文件中存储的故障日志文件:/tisdip_rk/state-v55k/exit-exit-gin:meta v/cc4.crack/ccip_gfut/j-fichtisips/gip_gip_gip-gip-fic/j-fichtisip-fic/j-fcc 3.0.0034万 6.1 3.0.0034万 6.1 3.0.0034万

查看/tisdk/build/arago-tmp-external_linaro-toolchain/work /x86_64-6.1 3.0.0034万.3.0.0034万_install.log时,会重复出现6.1

2017年28月06日 08:47:37(GMT)- runEclipseApp -失败0:无法连接到Mir:无法连接到服务器套接字:没有此类文件或目录
无法初始化服务器:无法连接:连接被拒绝
Eclipse:无法打开显示:2017年28月06日
08:47:37(GMT)- EclipseApp -错误代码: CHILDKILLED 1.5671万 SIGSEGV {segmentation violation } 2017年28月06日
08:47:37(GMT)- runEclipseApp - Running again 2017年28月06日
08:47:47(GMT)- runEclipseApp - Failed 1: Failed to connect to Mir: failed to server socket: No such file or directory
unable to init server: could not connect: could connect: Connection refused Eclipse
:Connection refused:Cannot opened Eclipse: Cannot open display:
2017年28月06日 08:47:47 (GMT)- runEclipseApp -错误代码:CHILDKILLED 1.9478万 SIGSEGV{Segmentation Violation}2017年28月06日
08:47:47 (GMT)- runEclipseApp - Running Again 2017年28月06日
08:47:58 (GMT)- runEclipseApp - Failed 2:Failed to connect to Mir:Failed to connect to server socket:no such file or directory (无法连接到服务器套接字):无此类文件或目录) 

等等。我附上了完整的日志以供参考。

e2e.ti.com/.../1108.ccs_5F00_setup_5F00_6.1.3.0.0034万_5F00_install.log

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    顺便说一下,我的主机是Ubuntu 16.04 LTS 64位。

    删除所有内容并重新开始会出现一些略有不同的错误。 这次似乎找不到一些库。

    2017年28月06日 13:59:51 (GMT)-验证::linuxLibChecks - LD_LIBRARY_PATH ==:/tmp/CCS_d9.5742万be-8096-4411-6873-8bb5b1196ad0/TCL/lib</s>8096 441168731196
    2017年28月06日 check_depends.sh 2017年28月06日 13:59:51(GMT)-验证:linuxLibCheckerChecknks - tempLD =={} 2017年28月06日 check_depends.sh 2.23 13:59:51(GMT)-验证:linuxcmdLibks -验证=/tmp/mcs_d9.5742万be-8096-4411-6873-8bb5b1196ad0/dependencion-libxcmdbcdcmks=13:/tmp_d9574gcmx_d55-libg42gcmx-x:libg9d55/libgcmx-8cmx:libg42bx-8cmx-8bx-libd57d55:libgb<xmt-block2>8096 2017年28月06日4411 2017年28月06日</xmt-block>6873 的1196 的依赖9574依赖关系2017关系:1cmx-1cmx-1cmx-1d55-8bx-8bx-8bx-d57d55d55d55d7d7d7d55:libgb:: glibc_glibc_glibcXX_glibcXX_19 2.11 正在检查ext-depends.txt中库的可用性... 3.4 找不到libasound.so.2 找不到libbatk-libbers.so.0 1.0 找不到libcairo.so.2 找不到libcups.so.2 找不到libdbus-1.so.3 找不到libdbus-glib-1.so.2 找不到libdbus-1.so.2没 能找到libto:libtlibe.so.6没能找到lib.libso:libe.libso.libto:libto.libso.lib.libto:lib.libto:libso.lib.lib.libto:libto:libso.lib.lib.libso.lib.libto.lib.libso.2找不到 libgconf-2.so.4 未能找到libgcrypt.so.11 未能找到libgdk_pixbuf-libgs.so.0 未能找到libgdk-x11-libglib.so.0 2.0 未能找到libgfs-libglib.lib.lib.libgfs-lib.so.0 未能找到libglibglib.lib.lib.lib.lib.so.0未能找到2.0 2.0 2.0 2.0 ,2.0 未能找到2.0 libgtk-x11-libor.so.0 2.0 找不到libpango-lib.so.6 找不到lib: libncurses.so.5 找不到liborBit-2.so.0 找不到libo:libpango-lib.so.0 1.0 找1.0 不到libplib.x1.lib.lib.lib.x1.lib.lib.lib.lib.x1.smo:libp 找 不到libpangocair-lib.x1.lib.lib.x1.lib.lib.x1.sm.lib.lib.x1.lib.lib.lib.lib.lib.lib.x1.lib.lib.lib.x1.sm.lib.lib.lib.lib.lib.lib.x1.sm.lib.to:找不到1.0 找不到 libXdamage.so.1 找不到libXext.so.6 找不到libXfixes.so.3 找不到libXi.so.6 找不到libxml2.so.2 找不到libXrandr.so.2 找不到libXrandr.so.2找 不到libXrender .so.1找不到libXt.libx.libxt.so.1找 不到libXt. 2017年28月06日 2.11 13:59:55(GMT)-验证:linuxLibChecks -行:安装的glibc和glibcxx: glibc_Glibc_Glibc, N/A 2017年28月06日 13:59:55(GMT)-验证::linuxLibChecks -行:glibc和glibcxx: 2.23 3.4 的必需版本:2017年28月06日 行验证:19 ext-depends.txt::13: 2017年28月06日 13:59:55 (GMT)-验证:linuxLibChecks -行:未能找到lib: libasound.so-2 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibuxks - Val:libasound.so-2 2017年28月06日 13:59:55 (GMT)-验证:Linuxlinliks -行:未能找到Libuxlib.batks - 1.0 2017年28月06日 :0:0:0:0:1.0 :0:0:0: libcairo.so.2 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks - Val:libcio.so.2 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks -行:未能找到libcups.so.2 2017年28月06日 13:59:55 (GMT) liblinuxChecks库- 2017年28月06日 3.59:1.13.0:1::1.59 (2017年28月06日 :13.0:13: 未能找到libdbus-glib-1.so.2 2017年28月06日 2017年28月06日 13:59:55(GMT)-验证:linuxChecks - Val:libdbus-glib-1.so.2 2017年28月06日 2017年28月06日 13:59:55(GMT)- 验证:linuxCheckks -行:未能找到liblinuxChecks.so.1 2017年28月06日 13:59:gmtvl -未能找到liblinux13.59:gvl:val:5.59:gt -val:val:13.59:gt libfontconfig.so.1 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks -行:未能找到库:libfreetype.so.6 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks - Val:libfreetlib.so.6 2017年28月06日 13:59 (GMT)验证:行:未能找到2017年28月06日 13.x8.59 (13: libgcrypt.so.11 2017年28月06日 13:59:55 (GMT)-验证::linuxLibxChecks - Val:libgcrypt.so.11 2017年28月06日 2.0 2017年28月06日 13:59:55 (GMT)-验证::linuxLibxChecks -行:未能找到库:libgdk_libxpixbuf-kx.0 2017年28月06日 2.0 2017年28月06日 13:libxuxvdk:gvl :gv-5.59 (2.0 :vl:vl: gx5.59)验证:xvl:gxvl:gxvl:gv-5.59:gvl:gxv-vl:gv-v-5.59 2017年28月06日 -验证:gxvl:gxvl:gx5.59:gxvl:vl:gx5.59 2.0 -验证-vl:x5.59:gxvl:gt 5.59 -验证:x5.59 -验证:xvl:x5.59:xvl:gt 5.59:gt 未能找到库:libgio-2.0 .so.0 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks-Val:libgio-2.0 .so.0 2017年28月06日 13:59:55 (GMT)-验证::2.0 -行:未能找到liblib:libglib-2.0 2017年28月06日 .so.0 2017年28月06日 13:59 (2.0 2017年28月06日 : libgmodule-linuxChecks.so.0 2017年28月06日 2.0 2017年28月06日 13:59:55(GMT)-验证2017年28月06日 Checks - lib: libgnomevfs-2.so.0找不到libgnomevfs-2.so.0 2017年28月06日 13:59:55(GMT)-验证:linuxLibxChecks - libglinks: libgnomevfs-2.so.0 2.0 2017年28月06日 2.0 13:59:gval -找到: libgthread-libChecks.so.0 2017年28月06日 2.0 2017年28月06日 13:59:55 (GMT)-验证::2.0 Checks - Val:libgthread-libxChecks.so.0 2017年28月06日 13:59:55 (GMT)-验证::2017年28月06日 -行:未 能找到libgtk-x11-libx5.59 (2.0 :libx5.59) libxliks:2017年28月06日 : 6.13::lux13:lux6:2.0 2017年28月06日 :libx5.59:libxwl: 未能找到libncurses.so.5 2017年28月06日 2017年28月06日 13:59:55(GMT)-验证:linuxLibChecks - Val:libncurses.so.5 2017年28月06日 1.0 13:59:55(GMT -验证:linuxLibChecks -行:未能找到liborBit-2.so.0 2017年28月06日 13:59:55(GMT) LibuxChecks 2017年28月06日 -验证:0.GMT:0 -:0 :0库:0库 :库:库:库: libpango-LibChecks.so.0 2017年28月06日 1.0 2017年28月06日 13:59:55 (GMT)-验证::1.0 Checks -行:未能找到libpangocairo-Libux.so.0 2017年28月06日 13:59:55 (GMT)-验证::1.0 1.0 2017年28月06日 linuxChecks - libpangocairo-liblinux.so.0 2017年28月06日 13:59:1.0 -未能找到:13: libsm.so.6 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks - Val:libsm.so.6 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks - 行:未能找到liblib:libX11.so.6 2017年28月06日 13:59:55 (GMT)- 2017年28月06日 8.59:8.59 (GMT)复合Libux:13.59:13:13: 未能找到libXdamage.so.1 2017年28月06日 13:59:55(GMT)-验证:linuxLibChecks - Val:libXdamage.so.1 2017年28月06日 2017年28月06日 13:59:55(GMT -验证:linuxChecks -行:未能找到liblib: libXext.so.6 2017年28月06日 13:59:55(GMT)-验证 :Libux: 2017年28月06日 :6.Val: 3.59: libxval: libXfixes.so.3 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks -行:找不到库:libxy.so.6 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxLibChecks - 库:libxy.so.6 2017年28月06日 13:59:55 (GMT)-验证:linuxLibxLibxChecks -未能找到libxval:2.59 (行:2:2017年28月06日 :2.59) libxrandr.so.2 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxChecks - Val:libxrandr.so.2 2017年28月06日 2017年28月06日 13:59:55 (GMT)-验证::linuxChecks -行:未能找到库:libxrender .so.1 2017年28月06日 13:59:2017年28月06日 (GMT)验证:libx18 :5.59 (linux:lint)验证:libx5.59:x5.59 (GMT::lint 5.59)验证-未能找到库6::x5.59 (:x5.59:l∶lint 13:x5.59 (linux:lint验证:x5.59)验证:x13:lint:x5.59:x13:lint:x5.59:xt验证:x5.59 (GMT:l0)验证:xb:xb:xt验证:x5.59 (:x5.59:l 找不到库:libXtst.so.6 2017年28月06日 13:59:55(GMT)-验证::linuxLibChecks - Val:libXtst.so.6 2017年28月06日 13:59:55(Gra)-验证::linuxLibChecks -行:找不到库:libcanuxChecks.so.0 2017年28月06日 13:59:55(GMT)-验证 :libanuxberra:0:2017年28月06日 :完成

    缺少的库似乎存在于/usr/lib/x86_64-linux-GNU中,但它没有正确找到它们。

    同样,请完整记录attachede2e.ti.com/.../2043.ccs_5F00_setup_5F00_6.1.3.0.0034万_5F00_install.log

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,
    您运行的是哪个版本的Linux内核? 我想知道您是否遇到了以下问题:
    e2e.ti.com/.../222.6461万

    它不仅会影响CCS GUI,还会构建任何基于RTSC的项目

    Thansk
    KI
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    忽略我的最后一条消息。 我错过了你的第二篇帖子。 我正在调查你第二篇文章中的信息
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您是否安装了以下链接中提到的依赖性?
    processors.wiki.ti.com/.../Linux_Host_Support_CCSv6
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢!  Yocto版本(CCS是内置的)在我在较旧的内核下运行时已经完成,所以segfault肯定是内核错误造成的。 但是,使用链接中提到的环境变量不起作用,因此我认为这些设置在生成过程的某个位置被覆盖。

    是,已安装依赖关系。 我认为库未链接的一个可能原因是,在安装时创建的/tmp/mcS./dpenedcy-checker文件夹中,从未出现名为ldcheck的文件。 它试图作为所附日志中Validation::linuxLibChecks阶段的一部分运行。 目前,我认为缺少的库不是问题,因为根据CCS构建的Yocto步骤似乎已正确完成。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    正在运行

    ~$ sudo apt-get install libc6:i386 libx11-6:i386 libastoundunzip:liblibliblibliblibibbus-glib-i386-2 1.0 :libglibconf-2-4:i386 2 gcrypt20:i386 libgdk-i386 libbit2:2.0 6:libbuc-libli-liblik-liblip-3i386-libtr-libtr-liblip-liblik-liblip-liblip-liblik-3i386 0.1 :1.0 i386-liblik-libliblik-liblip-liblip-liblik-liblik-1i386-liblik-liblip-libtri386-liblik-liblik-liblik-liblik-1i386-liblik-libtri386

    提供

    正在读取软件包列表... 完成
    生成依赖关系树
    正在读取状态信息... 完成
    Unzip已经是最新版本(6.0 -20ubuntu1)。
    libasound2:i386已经是最新版本(1.1 .0-0ubuntu1)。
    libat千 分1.0 -0:i386已是最新版本(2.18 .0-1)。
    libcairo2:i386已经是最新版本(1.14 .6-1)。
    libcanberra-gtk-module:i386已经是最新版本(0.30 -2.1ubuntu1)。
    libcups2:i386已经是最新版本(2.1 .3-4)。
    libdbus-glib-1-2:i386已经是最新版本(0.106 -1)。
    libgconf-2-4:i386已经是最新版本(3.2 .6-3ubuntu6)。
    libgnomeui-0:i386已经是最新版本(2.24 .5-3.1)。
    libice6:i386已经是最新版本(2:libice.9-1 1.0)。
    libncurses5:i386已经是最新版本(6.0 + 2016.0213万-1ubuntu1)。
    liborbit2:i386已经是最新版本(1:libor.19-1build1 2.14)。
    libsm6:i386已经是最新版本(2:1.2 .2-1)。
    libusb-libus-4:i386 0.1 已经是最新版本(2:0.1 .12-28)。
    libusb-libus-0-dev 1.0 :i386已经是最新版本(2:1.0 .20-1)。
    libx11-6:i386已经是最新版本(2:1.6 .3-1ubuntu2)。
    libxt6:i386已经是最新版本(1:1.1 .5-0ubuntu1)。
    libxtst6:i386已经是最新版本(2:libxtst.2-1 1.2)。
    GTK2-INGS-MOURINE:i386已经是最新版本(0.98 .2-0ubun里 瓦尔2.2)。
    libc6:i386已经是最新版本(2.23 -0ubuntu9)。
    libgcrypt20:i386已经是最新版本(1.6 .0.2)。
    libgdk-pixbu384-0:i386 2.0 已经是最新版本(2.32 .2-1.2)。
    libgtk-3-0:i386已经是最新版本(3.18 .9-1ubunibu.3.3)。
    libstdc++6:i386已经是最新版本(5.4 .0-6ubuntu1~16.04 .4)。
    libudev1:i386已经是最新版本(229-4ubuntu17)。

    和~$locate libatk

    /usr/lib/x86_64-linux-gnu/libatk-libatk-1.0 .so.0
    /usr/lib/x86_64-linux-GNU/libatk-libatk- 1.0 .so.0.2.1809万 .1.
    /usr/lib/x86_64-linux-gnu/libatk-bridge-2.0 .so.0
    /usr/lib/x86_64-linux-gnu/libatk-bridge-2.0 .so.0.0 .0
    /usr/lib/x86_64-linux-gnu/libatkmm-linux.so 1.6 .1
    /usr/lib/x86_64-linux-GNU/libatkmm-libat.so 1.6 .1.1 .0
    /usr/lib/x86_64-linux-gnu/gtk-modules/libatk-bridge 2.0 .so
    /usr/share/doc/libatk-adaptor
    /usr/share/doc/libatk-bridgee 2.0 -0
    /usr/share/doc/libat千 分之1.0 -0
    /usr/share/doc/libat千1.0 -data
    /usr/share/doc/libatkmm-libatkmm-1v5 1.6
    /usr/share/doc/libatk-adapter/NEWS.gz
    /usr/share/doc/libatk-adapter/README
    /usr/share/doc/libatk-adapter/changelog.Debian.gz
    /usr/share/doc/libatk-adapter/copyright
    /usr/share/doc/libatk-bridgee 2.0 -0/changelog.Debian.gz
    /usr/share/doc/libatk-bridgee 2.0 -0/copyright
    /usr/share/doc/libat千 米1.0 -0/authors
    /usr/share/doc/libat千 米1.0 -0/NEWS.gz
    /usr/share/doc/libat千 米1.0 -0/README
    /usr/share/doc/libat千 米1.0 -0/changelog.Debian.gz
    /usr/share/doc/libat千 分之1.0 -0/copyright
    /usr/share/doc/libat千 分之1.0 -数据/作者
    /usr/share/doc/libat千 分之1.0 -data/NEWS.gz
    /usr/share/doc/libat千 米1.0 数据/README
    /usr/share/doc/libat千 分之1.0 -data/changelog.Debian.gz
    /usr/share/doc/libatbid千 米1.0 -数据/版权
    /usr/share/doc/libatkmm-libatkmm-v5/authors 1.6
    /usr/share/doc/libatkmm-usp-1v5/NEWS.gz 1.6
    /usr/share/doc/libatkmm-README 1.6
    /usr/share/doc/libatkmm-usp-1v5/changelog.Debian.gz 1.6
    /usr/share/doc/libatkmm-copyright 1.6
    /var/cache/apt/archives/libatk-bridgee 2.0 -2.18 0_.1-2ubuntu1_i386.deb
    2.18.0-1_i386.deb 1.0
    /var/lib/dpkg/info/libatk-adaptor:amd64.conffiles
    /var/lib/dpkg/info/libatk-adaptor:amd64.list
    /var/lib/dpkg/info/libatk-adaptor:amd64.md5sums
    /var/lib/dpkg/info/libatk-bridgee 2.0 -0:amd64.list
    /var/lib/dpkg/info/libatk-bridgee 2.0 -0:amd64.md5sums
    /var/lib/dpkg/info/libatk-bridgee 2.0 -0:amd64.shlibs
    /var/lib/dpkg/info/libatk-bridgee 2.0 -0:amd64.symbols
    /var/lib/dpkg/info/libatk-bridgee 2.0 amd64-0:amd64.triggers
    /var/lib/dpkg/info/libatbersquid-0:amd64.list 1.0
    /var/lib/dpkg/info/libatbersquid-0:amd64.md5sums 1.0
    /var/lib/dpkg/info/libatbish-0:amd64.shlibs 1.0
    /var/lib/dpkg/info/libatbersquid-0:amd64.symbols 1.0
    /var/lib/dpkg/info/libatbersquid-0:amd64.triggers 1.0
    /var/lib/dpkg/info/libatbidci-data.list 1.0
    /var/lib/dpkg/info/libatbersquid-data.md5sums 1.0
    /var/lib/dpkg/info/libatkmm-amd64.list 1.6
    /var/lib/dpkg/info/libatkmm-amd64.md5sums 1.6
    /var/lib/dpkg/info/libatkmm-amd64.shlibs 1.6
    /var/lib/dpkg/info/libatkmm-amd64.triggers 1.6