This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] IcePick_C:初始化仿真器时出错:(错误-260 @ 0x0)

Guru**** 2927270 points

Other Parts Discussed in Thread: CC1352P

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1097229/icepick_c-error-initializing-emulator-error--260-0x0

主题中讨论的其他部件:CC1352P

各位专家,您好!

我尝试在Linux操作系统环境中执行Pin interrupt CC1352P示例。  

我在调试会话 IcePick_C上得到isuse:初始化仿真器时出错:(错误-260 @ 0x0)。

有人能帮我解决这个问题吗!

以下错误屏幕截图:

在常规中验证连接时。 我得到了这个  

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

/home/keerthivasan/.ti/ccs1120/1/0/BrdDat/
    testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100/110/510 class product.
This utility will load the adapter 'libjioxds110.so'.
The library build date was 'Mar 17 2022'.
The library build time was '15:40:16'.
The library package version is '9.7.0.00213'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.

[End]