This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] GUI Composer 中的串行端口配置至 XDS110类

Guru**** 2933120 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1045137/serial-port-configuration-in-gui-composer-through-xds110-class

您好!

我正在使用" ti-widget-optionsmenu" in Gui Composer, to build an IHM to control a mmWaveSensor.

The goal is to stream USB-UART datas coming from the sensor.

1- When using the "ti-widget-optionsmenu" from a blank page in Gui Composer, I get the following window :

2- When checking the "ti-widget-optionsmenu" coming from "mmWave_demo_Visualizer", I get :

It seems that, in this second case, the COM ports are streamed through a XDS110 Class.

And I think it is exactly what I would like to do.

My question is : how to get this configuration ? how to communicate with COM ports through XDS110 ?

Many thanks in advance for your help.

Bruno

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Bruno、

    我怀疑区别在于、文本是在毫米波演示可视化工具中修改的。 我将确认这一点、并在我有答案时回复您。

    谢谢

    Ki

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Ki、

    最后,我找到了对我的问题的答复。

    这是在 html 中对"index.GUI"的 gist 进行编程的问题。 我使用"ti-transport-usb"小工具添加了以下行:


    <ti-model-streaming id="CFG_port" protocol="cr" class="_TI_">


    <ti-model-streaming id="DATA_port" protocol="raw" class="_TI_">

    这解决了问题: gist 的编程优先于“属性”菜单的配置。 GUI Composer 的"property"菜单似乎不支持所有可能的目标配置。