This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 尝试构建时出现 LAUNCHCC3235MOD 错误#39;hello#39;示例

Guru**** 2878190 points

Other Parts Discussed in Thread: LAUNCHCC3235MOD, CC3235SF, SYSBIOS

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1021443/launchcc3235mod-errors-when-trying-to-build-hello-examples

主题中讨论的其他器件:LAUNCHCC3235MODCC3235SFSYSBIOS

您好!

我使用 的是 LAUNCHCC3235MOD launchpad。 当我尝试 构建 hello 示例工程时、我会看到两个工程的以下错误。  

CCS 版本: 10.4.0.00006  

**** Build of configuration MCU+Image for project hello_CC3235SF_LAUNCHXL_tirtos_gcc ****

"C:\\ti\\ccs1040\\ccs\\utils\\bin\\gmake" -k -j 8 all -O 
 
Building file: "../hello.cfg"
Invoking: XDCtools
"C:/ti/ccs1040/xdctools_3_62_01_15_core/xs" --xdcpath="C:/ti/simplelink_cc32xx_sdk_5_20_00_06/source;C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages;C:/ti/simplelink_cc32xx_sdk_5_20_00_06;" xdc.tools.configuro -o configPkg -t gnu.targets.arm.M4 -p ti.platforms.simplelink:CC32XX -r release -c "C:/ti/ccs1040/ccs/tools/compiler/gcc-arm-none-eabi-9-2019-q4-major" --compileOptions "-mcpu=cortex-m4 -march=armv7e-m -mthumb -mfloat-abi=soft -I\"C:/TI_Workspace/hello_CC3235SF_LAUNCHXL_tirtos_gcc\" -I\"C:/TI_Workspace/hello_CC3235SF_LAUNCHXL_tirtos_gcc/MCU+Image\" -I\"C:/ti/simplelink_cc32xx_sdk_5_20_00_06/source\" -I\"C:/ti/simplelink_cc32xx_sdk_5_20_00_06/source/ti/posix/gcc\" -I\"C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/include/newlib-nano\" -I\"C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/include\" -I\"C:/ti/ccs1040/ccs/tools/compiler/gcc-arm-none-eabi-9-2019-q4-major/arm-none-eabi/include\" -ffunction-sections -fdata-sections -g -gstrict-dwarf -Wall  -std=c99 " "../hello.cfg"
subdir_rules.mk:19: recipe for target 'build-1057507295-inproc' failed
/usr/bin/sh: 0: Can't open C:/Users/KEOND~1/AppData/Local/Temp/make17624-1.sh
C:/ti/ccs1040/xdctools_3_62_01_15_core/packages/xdc/bld/xdc_rules.mak:307: *** Error: Specified build configuration file '' is not found.  Stop.
js: "C:/ti/ccs1040/xdctools_3_62_01_15_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[1]: *** [build-1057507295-inproc] Error 1
Building file: "../image.syscfg"
Invoking: SysConfig
"C:/ti/ccs1040/ccs/utils/sysconfig_1.9.0/sysconfig_cli.bat" -s "C:/ti/simplelink_cc32xx_sdk_5_20_00_06/.metadata/product.json" --script "C:/TI_Workspace/hello_CC3235SF_LAUNCHXL_tirtos_gcc/image.syscfg" -o "syscfg" --compiler gcc
Running script...
Validating...
Generating Code (image.syscfg)...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\RegDomainSum5.csv...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\RegDomainSum24.csv...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_drivers_net_wifi_config.json...
Finished building: "../image.syscfg"
 
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/linker.cmd'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
 
Building file: "../hello.syscfg"
Invoking: SysConfig
"C:/ti/ccs1040/ccs/utils/sysconfig_1.9.0/sysconfig_cli.bat" -s "C:/ti/simplelink_cc32xx_sdk_5_20_00_06/.metadata/product.json" --script "C:/TI_Workspace/hello_CC3235SF_LAUNCHXL_tirtos_gcc/hello.syscfg" -o "syscfg" --compiler gcc
Running script...
Validating...
Generating Code (hello.syscfg)...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_drivers_config.c...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_drivers_config.h...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_utils_build_linker.cmd.genlibs...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\syscfg_c.rov.xs...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_utils_runtime_model.gv...
Writing C:\TI_Workspace\hello_CC3235SF_LAUNCHXL_tirtos_gcc\MCU+Image\syscfg\ti_utils_runtime_Makefile...
Finished building: "../hello.syscfg"
 
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-1057507295', needed by 'configPkg/compiler.opt'.
 
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

我导入它们的方式是:

项目

导入 CCS 工程

搜索目录是 SDK 的位置

我是否遗漏了什么?  

提前感谢您。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我不确定是什么问题 、需要咨询 CCS 专家。  

    您是否更改了项目属性中的任何内容?  

    CCS 编译是否适合您?

    BR、

    Kobi

    ****为项目 hello_CC3235SF_LAUNCHXL_tirtos_gcc 构建配置 MCU+Image ****

    "C:\\ti\\ccs1040\\ccs\\utils\\bin\\gmake"-k -j 12 all -O

    编译文件:"../hello.cfg"
    调用:XDCtools
    "c:/ti/ccs1040/xdctools_3_62_01_15_core/xs "--xdcpath="C:/ti/simplelink_cc32xx_sdk_5_20_00_06/source;C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages;C:/ti/simplelink_cc32xx_sdk_5_20_00_06;" xdc.tools.configuro configPkg -t GNG.targets.arm.M4 -p ti.platforms.simplelink:CC32XX /Users/a0798996/workspace/workspace_5.20/hello_CC3235SF_LAUNCHXL_tirtos_gcc/MCU /ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/include/newlib-nano -r release -c "C:/ti/ccs1040/ccs/tools/compiler/gcc-arm-none-eabi-7-2017-q4-major-win32 -compileOptions "-mcpu=cortex-M4 -March \armv7e-m -mb -chumb -/Users/a0798996/workspace/workspace_5.20/hello_CC3235SF_LAUNCHXL_tirtos_gcc /ti/simplelink_cc32xx_sdk_5_20_00_06/source/ti/posix/gcc /ti/ccs1040/ccs/tools/compiler/gcc-arm-none-eabi-7-2017-q4-major-win32/arm-none-eabi/include -chines"-c "c:/ti/simplelink_cc32xx_sdk_5_20_00_06/source /ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/include -dstd i:/dfb -ab"-dstd i -ab"-mb -mb -mscrultrab-df -mb -df -df -df -df -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mb -mcr -mcr -mcr
    正在制作 package.mak (由于 package.bld)...
    正在为软件包 configPkg 生成接口(因为 package/package.xdc.inc 比 package.XDC 旧)...
    从 package/cfg/hello_pm4g.cfg 配置 hello.xm4g ...
    正在生成自定义 ti.sysbios 库 makefile ...
    正在开始构建库源...
    制作 C:/Users/a0798996/workspace/workspace_5.20/hello_CC3235SF_LAUNCHXL_tirtos_gcc/src/sysbios/sysbios.am4g ...
    asmm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm_gnu.sv7M……
    asmm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch_gnu.sv7M……
    asmm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm_gnu.sv7M……
    asmm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/TaskSupport_asm_gnu.sv7M……
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/BIOS.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Clock.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Idle.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Intrinsics.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Queue.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Semaphore.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Swi.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/knl/Task.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/hal/Hwi.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/hal/Hwi_stack.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/hal/Hwi_startup.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Hwi.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/TaskSupport.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/family/arm/m3/Timer.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/heaps/HeapMem.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/gates/GateHwi.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/gates/GateMutex.c
    clm4g C:/ti/simplelink_cc32xx_sdk_5_20_00_06/kernel/tirtos/packages/ti/sysbios/rts/gnu/ReentSupport.c
    arm4g m3_Hwi_ASM_GN0.o m3_Hwi_ASM_SWITCH_GN0.o m3_Intinsics.Support_ASM_TaskSupport_ASM_GN0.o _BIOS.o m3 L_Clock.o m3_Idle.o KNL_Intrinics.o KNL_Queu.o KNL_Rtog_Hwi_Semtagle.o Hwi_Hwi_Htask.o ngate.o m.h
    已完成库构建。
    clm4g 封装/cfg/hello_pm4g.c……
    完成构建:"../hello.cfg"

    已复制1个文件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="132163" URL"~/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1021443/launchcc3235mod-errors-when-trying-to-build-hello-examples/3775524 #3775524">您是否更改了项目属性中的任何内容?  [/报价]

    没有更改任何设置、我只是从资源中心安装了 CCS 和 SDK、然后导入了一个示例。  

    [引用 userid="132163" URL"~/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1021443/launchcc3235mod-errors-when-trying-to-build-hello-examples/3775524 #3775524"] CCS 编译是否适合您?

    CCS 编译对我无效。 我会得到相同的误差。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我测试过相同的测试、没有任何问题。

    唯一的区别是分别导入它们。

    可能会尝试删除当前项目、然后一次只导入 CCS 或 GCC。

    BR、

    Kobi

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我完全卸载了 CCS 和 SDK。 已重新安装、已从 Resource Explorer 中安装 SDK。 仅导入 hello CCS 版本、仍然收到相同的错误。  您能向我解释一下您的步骤吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我安装了最新的 SDK (来自 https://www.ti.com/tool/SIMPLELINK-CC32XX-SDK)并从其中导入了示例。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的、我能够使用一个解决安装了 Windows 的虚拟机的工作。 以相同的方式安装 CCS、并且工作正常。 我使用的是公司计算机、因此我想知道我的组织是否有设置阻止我正确使用 CCS。