Other Parts Discussed in Thread: CCSTUDIO
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
Thread 中讨论的其他器件:CCStudio您好!
我在 CCStudio v9.2.0中遇到类似的问题。 安装完美、但一旦启动、工作区就不会打开、并且像我在下面所连接的那样有空白白屏。 也会显示一条错误消息。

以下是错误日志:
eclipse.buildId=4.8.0.I20180611-0500
java.version=1.8.0_112
java.vendor=Oracle Corporation
BootLoader constants: OS=macosx, ARCH=x86_64, WS=cocoa, NL=en_US
Framework arguments: -product com.ti.ccstudio.branding.product -keyring /Users/pvj/.eclipse_keyring -showlocation
Command-line arguments: -os macosx -ws cocoa -arch x86_64 -product com.ti.ccstudio.branding.product -keyring /Users/pvj/.eclipse_keyring -showlocation
!ENTRY org.eclipse.ui.workbench 4 2 2021-08-27 17:54:12.795
!MESSAGE Problems occurred when invoking code from plug-in: "org.eclipse.ui.workbench".
!STACK 0
java.lang.NullPointerException
at org.eclipse.swt.widgets.Control.internal_new_GC(Control.java:2178)
at org.eclipse.swt.graphics.GC.<init>(GC.java:174)
at org.eclipse.swt.graphics.GC.<init>(GC.java:135)
at org.eclipse.jface.wizard.ProgressMonitorPart.initialize(ProgressMonitorPart.java:237)
at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:138)
at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:103)
at org.eclipse.ui.splash.BasicSplashHandler$AbsolutePositionProgressMonitorPart.<init>(BasicSplashHandler.java:50)
at org.eclipse.ui.splash.BasicSplashHandler.getBundleProgressMonitor(BasicSplashHandler.java:138)
at org.eclipse.ui.splash.BasicSplashHandler.getContent(BasicSplashHandler.java:237)
at org.eclipse.ui.internal.splash.EclipseSplashHandler.init(EclipseSplashHandler.java:107)
at org.eclipse.ui.internal.Workbench$2.run(Workbench.java:872)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
at org.eclipse.ui.internal.Workbench.createSplashWrapper(Workbench.java:887)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:631)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:597)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:148)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:656)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:592)
at org.eclipse.equinox.launcher.Main.run(Main.java:1498)
!ENTRY org.eclipse.ui 4 0 2021-08-27 17:54:12.801
!MESSAGE Could not instantiate splash
!STACK 0
java.lang.NullPointerException
at org.eclipse.swt.widgets.Control.internal_new_GC(Control.java:2178)
at org.eclipse.swt.graphics.GC.<init>(GC.java:174)
at org.eclipse.swt.graphics.GC.<init>(GC.java:135)
at org.eclipse.jface.wizard.ProgressMonitorPart.initialize(ProgressMonitorPart.java:237)
at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:138)
".log" 11207L, 855755B
请帮助。 我正在使用 macOS Big Sur 版本: 11.5.2
谢谢、
Prakhar