大家好,
如何针对 GCC 问题生成 ti rtos (tirtos_cc13xx_cc26xx) makefile (丢失 ti.platforms.simplelink),redirect 分配软件包?
1.在我的环境中
C:\ti\xdctools_3_32_00_06_core>gmake -f C:\ti_tirtos_cc13xx_cc26xx_2_21_01_08\tirtos.示 例 mak gen="c:\temp"
在 c:\temp...中生成示例
秘书长的报告
请参阅 TI-RTOS 中的"TI-RTOS 示例"部分
"入门指南"、了解有关如何构建和加载示例的详细信息
IAR 工作平台和 CCS 中。
C:\temp\examples\GNU\CC2650_LAUNCHXL\empty>make
正在运行 Configuro...
JS:"c:/ti/xdctools_3_32_00_06_core/packages/xdc/tools/Cmdr.xs、第51行:错误:xdc.tools.configuro:错误:找不到平台包'ti.platforms.simplelink'。 TI 平台不再作为 XDCtools (c:\ti\xdctools_3_32_00_06_core)的一部分提供。 请确保您使用的是3.30之前版本的 XDCtools、或者您添加了一个包含您的平台支持的产品、路径为"C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/tidrivers_cc13xx_cc26xx_2_21_01_01/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/bios_6_46_01_38/packages;C:/ti/tirtos_cc13xx_cc26xx_2_21_01_08/products/uia_2_01_00_01/packages;c:\ti\xdctools_3_32_00_06_core/packages。 检查此路径是否为包含必要平台支持的目录命名,以及平台名称是否拼写正确。
make:***[makefile:53:empty/linker.cmd]错误1.
2.
可以使用 gcc 来构建 cc13xx /ccc26xx 项目。
软件版本:
RTOS:
tirtos_cc13xx_cc26xx_2_21_01_08
simplelink:
BLE_SDK_2_02_05_02
CCS:
CCS v6.1.3
tirtos.mak
#
# ======== tirtos.mak ========
#
#
# Set location of various cgtools
#
# These variables can be set here or on the command line. Paths must not
# have spaces. If using a Windows PC, the following can be used to determine
# a directory's DOS path (path without spaces):
#
# 1. Open a command prompt.
# 2. Navigate (cd) into the directory.
# 2. Enter the following command:
# > for %I in (".") do echo %~sI
#
# The steps above should provide you with a path similar to the following:
# Original Path: c:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2
# DOS Path: c:\PROGRA~2\IARSYS~1\EMBEDD~1.2
#
# The final step is to replace all backslashes '\' in the path with forward
# slashes '/'.
# Correct Path: c:/PROGRA~2/IARSYS~1/EMBEDD~1.2
#
DEFAULT_INSTALL_DIR ?= c:/ti
CCS_COMPILERS_DIR ?= $(DEFAULT_INSTALL_DIR)/ccsv6/tools/compiler
#
# Enable TI-RTOS to build for CCS.
# Set CCS_BUILD to true and modify path to toolchain
#
CCS_BUILD ?= false
TI_INSTALL_DIR ?= $(CCS_COMPILERS_DIR)
ti.targets.arm.elf.M3 ?= $(TI_INSTALL_DIR)/gcc-arm-none-eabi-4_9-2015q3
#
# Enable TI-RTOS to build for IAR.
# Set IAR_BUILD to true and modify path to toolchain.
#
# The IAR_INSTALL_DIR must be set to point to the
# "Embedded Workbench x.y" directory in IAR Workbench. This path MUST NOT
# contain spaces. If using a Windows PC, see the comments above for steps to
# get the DOS path for a directory.
#
IAR_BUILD ?= false
IAR_INSTALL_DIR ?= c:/iar
iar.targets.arm.M3 ?= $(IAR_INSTALL_DIR)/arm
#
# Enable TI-RTOS to build for GCC.
# Set GCC_BUILD to true and modify path to toolchain
#
GCC_BUILD ?= true
GCC_INSTALL_DIR ?= $(CCS_COMPILERS_DIR)
gnu.targets.arm.M3 ?= $(GCC_INSTALL_DIR)/gcc-arm-none-eabi-6-2017-q1-update
#
# TI-RTOS and XDCTools settings
#
XDCTOOLS_INSTALL_DIR ?= $(DEFAULT_INSTALL_DIR)/xdctools_3_32_00_06_core
export XDCTOOLS_JAVA_HOME ?= $(DEFAULT_INSTALL_DIR)/ccsv6/eclipse/jre
TIRTOS_INSTALL_VER ?= tirtos_cc13xx_cc26xx_2_21_01_08
TIRTOS_INSTALL_DIR ?= $(DEFAULT_INSTALL_DIR)/$(TIRTOS_INSTALL_VER)
TIDRIVERS_INSTALL_DIR ?= $(TIRTOS_INSTALL_DIR)/products/tidrivers_cc13xx_cc26xx_2_21_01_01
BIOS_INSTALL_DIR ?= $(TIRTOS_INSTALL_DIR)/products/bios_6_46_01_38
UIA_INSTALL_DIR ?= $(TIRTOS_INSTALL_DIR)/products/uia_2_01_00_01
CC13XXWARE_INSTALL_DIR ?= $(TIRTOS_INSTALL_DIR)/products/cc13xxware_2_04_03_17272
CC26XXWARE_INSTALL_DIR ?= $(TIRTOS_INSTALL_DIR)/products/cc26xxware_2_24_03_17272
TIRTOS_PACKAGES_DIR ?= $(TIRTOS_INSTALL_DIR)/packages
TIDRIVERS_PACKAGES_DIR ?= $(TIDRIVERS_INSTALL_DIR)/packages
BIOS_PACKAGES_DIR ?= $(BIOS_INSTALL_DIR)/packages
UIA_PACKAGES_DIR ?= $(UIA_INSTALL_DIR)/packages
#
# Set XDCARGS to some of the variables above. XDCARGS are passed
# to the XDC build engine... which will load tirtos.bld... which will
# extract these variables and use them to determine what to build and which
# toolchains to use.
#
# Note that not all of these variables need to be set to something valid.
# Unfortunately, since these vars are unconditionally assigned, your build line
# will be longer and more noisy than necessary (e.g., it will include CC_V5T
# assignment even if you're just building for C64P).
#
# Some background is here:
# rtsc.eclipse.org/.../Command_-_xdc
#
XDCARGS= \
profile=release \
XDCTOOLS=$(XDCTOOLS_INSTALL_DIR) \
TIRTOS=$(TIRTOS_INSTALL_DIR) \
TIDRIVERS=$(TIDRIVERS_INSTALL_DIR) \
BIOS=$(BIOS_INSTALL_DIR) \
UIA=$(UIA_INSTALL_DIR) \
CC13XXWARE=$(CC13XXWARE_INSTALL_DIR) \
CC26XXWARE=$(CC26XXWARE_INSTALL_DIR)
ifeq ("$(CCS_BUILD)", "true")
XDCARGS += \
ti.targets.arm.elf.M3=$(ti.targets.arm.elf.M3)
endif
ifeq ("$(IAR_BUILD)", "true")
XDCARGS += \
iar.targets.arm.M3=$(iar.targets.arm.M3)
endif
ifeq ("$(GCC_BUILD)", "true")
XDCARGS += \
gnu.targets.arm.M3=$(gnu.targets.arm.M3)
endif
export XDCARGS
#
# Set XDCPATH to contain necessary repositories.
#
XDCPATH = $(TIRTOS_PACKAGES_DIR);$(TIDRIVERS_PACKAGES_DIR);$(BIOS_PACKAGES_DIR);$(UIA_PACKAGES_DIR);
export XDCPATH
#
# Set XDCOPTIONS. Use -v for a verbose build.
#
#XDCOPTIONS=v
export XDCOPTIONS
#
# Set XDC executable command
# Note that XDCBUILDCFG points to the tirtos.bld file which uses
# the arguments specified by XDCARGS
#
XDC = $(XDCTOOLS_INSTALL_DIR)/xdc XDCARGS="$(XDCARGS)" XDCBUILDCFG=./tirtos.bld
XS = $(XDCTOOLS_INSTALL_DIR)/xs
#######################################################
## Shouldn't have to modify anything below this line ##
#######################################################
help:
@ echo Makefile to build components within TI-RTOS
@ echo goal description
@ echo -----------------------------------------------------------------------------
@ echo all Builds SYS/BIOS, UIA, and TI-RTOS drivers
@ echo drivers Builds TI-RTOS drivers and other components in /packages
@ echo bios Builds SYS/BIOS
@ echo uia Builds UIA
@ echo clean Cleans SYS/BIOS, UIA, and TI-RTOS drivers
@ echo clean-drivers Cleans TI-RTOS drivers and other components in /packages
@ echo clean-bios Cleans SYS/BIOS
@ echo clean-uia Cleans UIA
@ echo examplesgen Generates TI-RTOS examples and makefiles
@ echo help Displays this description
all: bios uia drivers product
clean: clean-uia clean-drivers clean-bios clean-product
product:
@ echo building tirtos packages ...
@ $(XDC) -Pr ./packages
clean-product:
@ echo cleaning tirtos packages ...
@ $(XDC) clean -Pr ./packages
drivers:
@ echo building tirtos drivers...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(TIDRIVERS_INSTALL_DIR)/drivers.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_INSTALL_DIR=$(BIOS_INSTALL_DIR) \
$(XDCARGS) -C $(TIDRIVERS_INSTALL_DIR)
clean-drivers:
@ echo cleaning tirtos drivers...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(TIDRIVERS_INSTALL_DIR)/drivers.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_INSTALL_DIR=$(BIOS_INSTALL_DIR) \
$(XDCARGS) -C $(TIDRIVERS_INSTALL_DIR) clean
bios:
@ echo building bios ...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(BIOS_INSTALL_DIR)/bios.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_SMPENABLED=0 \
$(XDCARGS) -C $(BIOS_INSTALL_DIR)
clean-bios:
@ echo cleaning bios ...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(BIOS_INSTALL_DIR)/bios.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_SMPENABLED=0 \
-C $(BIOS_INSTALL_DIR) clean
uia:
@ echo building uia ...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(UIA_INSTALL_DIR)/uia.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_INSTALL_DIR=$(BIOS_INSTALL_DIR) \
$(XDCARGS) -C $(UIA_INSTALL_DIR)
clean-uia:
@ echo cleaning uia ...
@ $(XDCTOOLS_INSTALL_DIR)/gmake -f $(UIA_INSTALL_DIR)/uia.mak \
XDC_INSTALL_DIR=$(XDCTOOLS_INSTALL_DIR) \
BIOS_INSTALL_DIR=$(BIOS_INSTALL_DIR) \
-C $(UIA_INSTALL_DIR) clean
validate-paths:
ifneq (1, $(words $(ti.targets.arm.elf.M3)))
$(error Toolchain path must not have spaces, please update the TI_INSTALL_DIR variable.)
endif
ifneq (1, $(words $(iar.targets.arm.M3)))
$(error Toolchain path must not have spaces, please update the IAR_INSTALL_DIR variable.)
endif
ifneq (1, $(words $(gnu.targets.arm.M3)))
$(error Toolchain path must not have spaces, please update the GCC_INSTALL_DIR variable.)
endif
examplesgen: validate-paths
ifneq ("$(DEST)","")
@ echo generating examples in $(DEST) ...
ifeq ("$(CCS_BUILD)", "true")
@ $(XS) examples.examplesgen \
--productGroup="CC13XX_CC26XX" \
--toolchain="TI" \
--toolchainDir="$(ti.targets.arm.elf.M3)" \
--output="$(DEST)/examples"
endif
ifeq ("$(IAR_BUILD)", "true")
@ $(XS) examples.examplesgen \
--productGroup="CC13XX_CC26XX" \
--toolchain="IAR" \
--toolchainDir="$(iar.targets.arm.M3)" \
--output="$(DEST)/examples"
endif
ifeq ("$(GCC_BUILD)", "true")
@ $(XS) examples.examplesgen \
--productGroup="CC13XX_CC26XX" \
--toolchain="GNU" \
--toolchainDir="$(gnu.targets.arm.M3)" \
--output="$(DEST)/examples"
endif
@ echo ***********************************************************
@ echo Please refer to "Examples for TI-RTOS" section in the TI-RTOS
@ echo "Getting Started Guide" for details on how to build and load the examples
@ echo into IAR WorkBench and CCS.
else
@ echo Specify destination path like this: DEST="YOURPATH". Use UNIX style path "C:/examples"
endif