This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/CC2640R2F:我有两个 I2C 器件、一个是器件地址为7位0x6C [7:1]、加上读取和写入位、另一个是6位0x36 [7:2]、第二个位必须为写入0、加上读取和写入。 如果我按照手册操作、那么 I2C

Guru**** 2535630 points
Other Parts Discussed in Thread: CC2640R2F

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/916632/ccs-cc2640r2f-i-have-two-i2c-devices-one-is-the-device-address-is-7-bit-0x6c-7-1-plus-read-and-write-bits-and-the-other-device-address-is-6-bit-0x36-7-2-and-the-second-bit-must-be-write-0-plus-read-and-write-if-i-follow-the-m

器件型号:CC2640R2F

工具/软件:Code Composer Studio

我有两个 I2C 器件、一个是器件地址为7位0x6C [7:1]、加上读写位、另一个是6位0x36 [7:2]、第二个位必须是写0、加上读写。 如果我按照手册操作、那么与两个器件对应的 tid 指定的 I2C 地址是相同的0x6C、即如何解决这种情况。