This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/TM4C1294NCPDT:无法使用 SERGER J-Link 仿真器连接 TM4C1294NCPDT 目标

Guru**** 2826755 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/906615/ccs-tm4c1294ncpdt-failed-to-connect-tm4c1294ncpdt-target-using-serger-j-link-emulator

器件型号:TM4C1294NCPDT
主题中讨论的其他器件:DK-TM4C129X

工具/软件:Code Composer Studio

当我运行配置文件时、我获得输出:

Cortex_M4_0:GEL 输出:
内存映射初始化完成
Cortex_M4_0:错误:STAT [ JLINKARM_IsHalted()调用]失败!
Cortex_M4_0:20次尝试后无法确定目标状态

我的 Code Composer Studio 版本为9.0.0.00018。

有什么建议吗?

谢谢你。