This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/TMS570LS0914:无头构建有时不执行任何操作

Guru**** 2524550 points
Other Parts Discussed in Thread: CCSTUDIO

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/668520/ccs-tms570ls0914-headless-build-sometimes-do-nothing

器件型号:TMS570LS0914
Thread 中讨论的其他器件:CCStudio

工具/软件:Code Composer Studio

您好!

Windows 10上的最新 CSS 6.2

我自动在 Jenkins 上构建以构建项目我执行下一个命令

mkdir %CSS_workspace%

C:\ti\ccsv6\eclipse\eclipsec -noSplash -data %css_workspace%-application com.ti.ccstudio.apps.projectImport -ccs.location %DIR%\>%log%
如果%errorlever% neq 0、则退出/b %errorlever%

C:\ti\ccsv6\eclipse\clipsec -noSplash -data %css_workspace%-application com.ti.ccstudio.apps.projectBuild -ccs.projects %project%-ccs.configuration %target%-ccs.autoOpen -ccs.buildType incremental >>%log%

如果%errorlever% neq 0、则退出/b %errorlever%

 

有时最后一个命令不编译任何文件。 ERRORLEVEL 设置为0。 有日志文件:

--------------------------------------------------
正在从'C:/Jenkins/workspace/1_tx_unit_test_Debug/platform_tx/tx_unit_test 导入项目/'...


完成!

%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
CCS 无头构建正在启动... [2018年3月02日12:22:27星期五食用]
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%。%%

====================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================
预处理...


====================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================
正在构建...


构建配置调试项目 TX_UNIT_TEST **"C

:\\ti\\ccsv6\\utils\bin\\gmake"-k -j 8 all -O

**build finished **========================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================



CCS 无头构建完成! 
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    [引用 user="Vladimir Romanov">有时最后一个命令不会编译任何文件。 [/报价]

    它的运行方式类似于已经有一个最新的.out 文件。 您提到这种情况有时会发生。 您是否能够为该项目始终如一地重现它、或者在同一项目导入/构建序列中、有时会发生但有时不会发生?

    您是否出于某种原因锁定到 CCS 6.2中、或者是否愿意尝试最新的 CCS 7.4?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    没有输出文件。 我在构建前清理工作区。  

    更新到7.4后问题消失。