请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:UCD3138、 UCC28951、 UCC28950工具/软件:TI C/C++编译器
尊敬的先生
我想设计电流为7安培的300V 直流输出、输入为440V 交流电
请推荐合适的参考设计
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.