This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 来自 CCS12.4的 SysConfig 工程不能在 CCS12.5中正确编译/打开

Guru**** 2914580 points

Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/1297301/sysconfig-project-from-ccs12-4-doesn-t-build-open-properly-in-ccs12-5

主题中讨论的其他器件:SysConfig

我们的项目已在 CCS12.4中完善。 由于一些器件选择问题、在12.5中打开的同一项目无法生成:

**** Build Finished ****
Buildfile generation error occurred..
This project was created for a device not currently recognized - Cortex R.AM263x.AM263x_CC:
- Re-run CCS installer on your existing CCS location, ensure the Product Family for your device is selected, and proceed with installation if it wasn't.
- See 'Help > Check for Updates' to check if support for this device is available through a CCS update.
- Migrate the project to closest matching supported device by adjusting project properties.
- Or contact TI for support if using experimental silicon.
Build stopped..

注意、提供的建议无关紧要、因为我可以为 AM263x 编译示例工程。

我曾尝试在 SysConfig 部分中纠正该问题、但结果完全解决了。

看起来.syscfg 文件需要一些人工编辑、然后 CCS12.5才会接受。

谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    答案是手动按如下所示编辑.cproject 文件: