主题中讨论的其他器件:CC1354P10、 LP-XDS110
工具与软件:
您好!
我在使用 Code Composer Studio 和 Launch Pad LP-XDS110对 CC1354P10进行编程时遇到问题。
我在控制台中看到的错误是
IcePick_C: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 12.8.0.00189)
xdsdfu.exe
、但也失败了。