请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMP92066 如下图所示,指定的温度范围为-25至120°C,工作温度为-40至125°C。 我们需要更低的温度范围至-40°C,因此只需检查该规格。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如下图所示,指定的温度范围为-25至120°C,工作温度为-40至125°C。 我们需要更低的温度范围至-40°C,因此只需检查该规格。