This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TSW14J57EVM:错误"coldn't 获取 RX"的链接

Guru**** 2387830 points
Other Parts Discussed in Thread: TSW14J58EVM
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1077688/tsw14j57evm-error-couldn-t-get-the-link-up-for-rx

部件号:TSW14J57EVM
“线程:测试TSW14J58EVM”中讨论的其它部件

您好,

客户在使用此设备时遇到错误,请参阅下面的详细信息。

“我们有一台设备连接到另一台 AFE79XX 系列和 TSW14J57。 当我们运行 Latte 设置程序时,我们收到一个错误“无法获取 RX 的链接”
我们不知道这是因为我们按下了 AFE79XX 上的按钮(SW1重置和 SW2重置),因为它以前工作正常。  

请参阅日志文本。  

#======
#Executing .. AFE79xx/bringup/setup.py
#Start Time 2022-02-15 20:08:09.268000 
AFE79xxLibraryPG1p0
spi - USB Instrument created.
resetDevice
Purge
MPSSE mode set
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
#Done executing .. AFE79xx/bringup/setup.py
#End Time 2022-02-15 20:08:16.795000
#Execution Time = 7.52700018883 s 
#================ ERRORS:0, WARNINGS:0 ================#
#======
#Executing .. AFE79xx/bringup/devInit.py
#Start Time 2022-02-15 20:08:23.953000 
Power Card - USB Instrument created.
Reset the FPGA and try again.
Loaded Libraries
#Done executing .. AFE79xx/bringup/devInit.py
#End Time 2022-02-15 20:09:10.857000
#Execution Time = 46.9040000439 s 
#================ ERRORS:1, WARNINGS:0 ================#
#======
#Executing .. AFE79xx/bringup/AFE79xx_EVM_Mode7.py
#Start Time 2022-02-15 20:09:30.249000 
TXA cannot be enabled when TXB is disabled. Consider enabling TXB instead of TXA.
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 14745.6
laneRateFb: 14745.6
laneRateTx: 14745.6
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 14745.6
laneRateFb: 14745.6
laneRateTx: 14745.6
Device Initialization for ChipVersion: 2.0
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x20
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
Waiting for MACRO_DONE bit to go high, Count: 1
Got MACRO_ERROR : EXECUTION_ERROR
MACRO_OPCODE : 0x13 MACRO_NAME : POWER_UP_CALIB
Macro Error Status Interpretation is Undefined in MacroLib
ERROR INTERPRETATION is : Not Interpreted
###########Device DAC JESD-RX 0 Link Status###########
LOS Indicator for (Serdes Loss of signal) lane 0: 1
Serdes-FIFO error for lane 0: 1
LOS Indicator for (Serdes Loss of signal) lane 1: 1
Serdes-FIFO error for lane 1: 1
LOS Indicator for (Serdes Loss of signal) lane 2: 1
Serdes-FIFO error for lane 2: 1
LOS Indicator for (Serdes Loss of signal) lane 3: 1
Serdes-FIFO error for lane 3: 1
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0xff00
###################################
###########Device DAC JESD-RX 1 Link Status###########
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0x0
###################################
#Done executing .. AFE79xx/bringup/AFE79xx_EVM_Mode7.py
#End Time 2022-02-15 20:11:38.483000
#Execution Time = 128.233999968 s 
#================ ERRORS:23, WARNINGS:1 ================#
#======
#Executing .. AFE79xx/bringup/bringup.py
#Start Time 2022-02-15 20:14:10.114000 
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 14745.6
laneRateFb: 14745.6
laneRateTx: 14745.6
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 14745.6
laneRateFb: 14745.6
laneRateTx: 14745.6
Device Initialization for ChipVersion: 2.0
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x20
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
###########Device DAC JESD-RX 0 Link Status###########
LOS Indicator for (Serdes Loss of signal) lane 0: 1
Serdes-FIFO error for lane 0: 1
LOS Indicator for (Serdes Loss of signal) lane 1: 1
Serdes-FIFO error for lane 1: 1
LOS Indicator for (Serdes Loss of signal) lane 2: 1
Serdes-FIFO error for lane 2: 1
LOS Indicator for (Serdes Loss of signal) lane 3: 1
Serdes-FIFO error for lane 3: 1
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0xff00
###################################
###########Device DAC JESD-RX 1 Link Status###########
LOS Indicator for (Serdes Loss of signal) lane 0: 1
Serdes-FIFO error for lane 0: 1
LOS Indicator for (Serdes Loss of signal) lane 1: 1
Serdes-FIFO error for lane 1: 1
LOS Indicator for (Serdes Loss of signal) lane 2: 1
LOS Indicator for (Serdes Loss of signal) lane 3: 1
Serdes-FIFO error for lane 3: 1
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0xbf00
###################################
#Done executing .. AFE79xx/bringup/bringup.py
#End Time 2022-02-15 20:15:46.452000
#Execution Time = 96.3379998207 s 
#================ ERRORS:25, WARNINGS:1 ================#

请提前感谢。

此致,
五月纳德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,梅纳德,

    SW1是 AFE 的硬件重置信号。 SW2是板载 CPLD 的重置信号。  在运行配置脚本之前按 SW1和 SW2不会影响 EVM 的功能。  客户看到的错误不是预期的原因。

    我看到,当执行 AFE79xx_EVM-Mode7脚本时,会出现一些意外的日志“TXA cannot be enabled when TXB is disabled (禁用 TXB 时无法启用 TXA)”。 考虑启用 TXB 而不是 TXA。” 脚本似乎从默认更新。  

    您可以使用默认脚本测试它们吗? 如果客户修改了该脚本,他们是否可以提供该脚本供我们在 EVM 上进行测试?

    此外,我看到客户运行了 bringup.py 脚本。 我们建议使用此脚本及其设置,因为此脚本是为 TSW14J58EVM 创建的,不支持 TSW14J57。

    此致,

    大卫·查帕罗

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大卫,你好。

    刚刚收到客户的回复,请参见下面的详细信息。

     我已在手边解决了 TX 的错误。 我希望您查看日志文件的后面部分。 我们的主要错误是 RX。 您可以从我所附加的新日志文件中看到这一点。 因为我们使用两台不同的计算机检查了这一点,其中一台计算机有默认的 Latte 脚本。 但是问题(日志)几乎完全相同。 这就是为什么我不认为错误是由于脚本造成的。 我注意到,在尝试访问 ADC 页面 HSDC pro 的数据时,RX LED 指示灯未亮起。 我还附加了 HSDC pro 在尝试运行进程时显示的错误窗口。 如果你能帮我解决这个问题,我将不胜感激。

    e2e.ti.com/.../Lattelog-_2800_2_2900_.zip

    "

    此致,
    五月纳德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,梅纳德,

    客户在日志中看到的错误是两个 DAC JESD 链路,DAC JESD Rx 0和 DAC JESD Rx 1。 在运行脚本之前,他们是否设置了 HSDC Pro 以向 AFE 发送声音?  

    我已经创建了一份文档,介绍如何将 AFE79xxEVM 与 TSW14J57配合使用。 请让客户关注本文档,了解他们是否可以在 HSDC Pro 中捕获数据。

    该文档可从以下链接下载: https://tidrive.ext.ti.com/u/omcyWTHnMnywZzJe/e2dfc9f4-0e08-4b66-a9fb-446feb3a266f?l 

    此致,

    大卫·查帕罗