This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS124S08EVM:ADS124S08 EVM无法使用外部Linux处理器读取寄存器

Guru**** 2558250 points
Other Parts Discussed in Thread: ADS124S08

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1091437/ads124s08evm-ads124s08-evm-unable-to-read-registers-with-external-linux-processor

部件号:ADS124S08EVM
主题中讨论的其他部件:ADS124S08

您好,  

 

我将ASD124S08 EVM https://www.ti.com/tool/ADS124S08EVM上的JP1短接 ,以便可以使用另一个微控制器来控制它以开发Linux驱动程序,并且我无法读取或写入寄存器。

 

请参阅以下设置:

 

微控制器: nrf5340-dk

RTOS:Zephyr.

SDK:nrf SDK 1.8 .........0

SPI时钟:5MHz

 

尝试读回所有寄存器时。 我得到全零。  

 为了测试SPI读取寄存器操作,我有一个无限的while循环来读取数据速率寄存器。

下面是生成的波形:

如上所示,在发出RREAD命令后,似乎根本没有读取寄存器。  

请参阅下面的驱动程序源代码,请参阅ads124s08.c底部的宏和ads124s08_SPI.c中的SPI实现:  

ads124s08.c

#define DT_DRV_COMPAT ti_ads124s08
#include <init.h>
#include <sys/byteorder.h>
#include <sys/__assert.h>
#include <logging/log.h>

LOG_MODULE_REGISTER(ads124s08, CONFIG_SENSOR_LOG_LEVEL);
#include "ads124s08.h"

#include <devicetree.h>
#include <drivers/gpio.h>

#include <nrf.h>
#include <hal/nrf_gpio.h>

static const struct device *dev_start;
static const struct device *dev_reset;


// configure GPIO Pins for CS, Start and reset

static void init_gpio(void)   {

    int status;

    dev_reset = device_get_binding(ADS124S08_RESET_LABEL);
    if (dev_reset == NULL){ 
      LOG_ERR("dev_reset device_get_binding() failure.");
      return;
    }

    status = gpio_pin_configure(dev_reset, ADS124S08_RESET_PIN, GPIO_OUTPUT_ACTIVE); 
    if (status < 0){ 
      LOG_ERR("dev_reset gpio_pin_configure() failure.");
      return;
    }

	dev_start= device_get_binding(ADS124S08_START_LABEL);
    if (dev_start == NULL){ 
      LOG_ERR("dev_start device_get_binding() failure.");
      return;
    }

    status = gpio_pin_configure(dev_start, ADS124S08_START_PIN, GPIO_OUTPUT_ACTIVE); 
    if (status < 0){ 
      LOG_ERR("dev_start gpio_pin_configure() failure.");
      return;
    }

#ifndef CONFIG_ADS124S08_TRIGGER
	nrf_gpio_cfg_input(DRDY_PIN, NRF_GPIO_PIN_PULLUP); 
#endif 

}


static void ads124s08_set_start_pin(int STATE){ 
  gpio_pin_set(dev_start, ADS124S08_START_PIN, STATE);
}
static void ads124s08_set_reset_pin(int STATE){ 
  gpio_pin_set(dev_reset, ADS124S08_RESET_PIN, STATE);
}



static const struct sensor_driver_api ads124s08_driver_api = {
	// .attr_set = ads124s08_attr_set,
#if CONFIG_ADS124S08_TRIGGER
	.trigger_set = ads124s08_trigger_set,
#endif
	// .sample_fetch = ads124s08_sample_fetch,
	// .channel_get = ads124s08_channel_get,
};



static int ads124s08_reset(const struct device *dev){ 

#if ENABLE_SOFT_CONFIGS // software reset 

	struct ads124s08_data *ads124s08 = dev->data; 
	ctrl = ADS124S08_CMD_RESET;
	ads124s08_spi_cmd_send(dev, ctrl);

#else // hardware reset 
	

  	ads124s08_set_reset_pin(HIGH); 
	k_sleep(K_MSEC(100)); 
	ads124s08_set_reset_pin(LOW);
	k_sleep(K_MSEC(100)); 
	ads124s08_set_reset_pin(HIGH);
	k_sleep(K_MSEC(100)); 
	
	  
#endif 
	return 0; 

}

static int ads124s08_init(const struct device *dev)
{
	struct ads124s08_data *ads124s08 = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	int status;
	
	ads124s08->bus = device_get_binding(cfg->bus_name);
	if (!ads124s08->bus) {
		LOG_ERR("master not found: %s", cfg->bus_name);
		return -EINVAL;
	}

	cfg->bus_init(dev);

	init_gpio(); 

	//Reset Device 
	status = ads124s08_reset(dev); 

	uint8_t reg; 

	while (1){ 

		status = ads124s08->hw_tf->read_reg(dev,ADS124S08_REG_DATARATE, &reg ); 
		LOG_INF("ADS124S08_REG_DATARATE: %x", reg);

		k_sleep(K_MSEC(1000)); 

	} 


	if (status < 0){ 
		LOG_ERR("ads124s08_init(). Unable to read status register"); 

	}

	return 0;
}



#if DT_NUM_INST_STATUS_OKAY(DT_DRV_COMPAT) == 0
#warning "ADS124S08 driver enabled without any devices"
#endif
/*
 * Device creation macro, shared by ADS124S08_DEFINE_SPI() and
 */

#define ADS124S08_DEVICE_INIT(inst)					\
	DEVICE_DT_INST_DEFINE(inst,					\
			    ads124s08_init,				\
			    NULL,					\
			    &ads124s08_data_##inst,			\
			    &ads124s08_config_##inst,			\
			    POST_KERNEL,				\
			    CONFIG_SENSOR_INIT_PRIORITY,		\
			    &ads124s08_driver_api);

#define IS_LSM303AGR_DEV(inst) \
	DT_NODE_HAS_COMPAT(DT_DRV_INST(inst), st_lsm303agr_accel)

#define DISC_PULL_UP(inst) \
	DT_INST_PROP(inst, disconnect_sdo_sa0_pull_up)

/*
 * Instantiation macros used when a device is on a SPI bus.
 */

#define ADS124S08_HAS_CS(inst) DT_INST_SPI_DEV_HAS_CS_GPIOS(inst)

#define ADS124S08_DATA_SPI_CS(inst)					\
	{ .cs_ctrl = {							\
		.gpio_pin = DT_INST_SPI_DEV_CS_GPIOS_PIN(inst),		\
		.gpio_dt_flags = DT_INST_SPI_DEV_CS_GPIOS_FLAGS(inst),	\
		},							\
	}

#define ADS124S08_DATA_SPI(inst)						\
	COND_CODE_1(ADS124S08_HAS_CS(inst),				\
		    (ADS124S08_DATA_SPI_CS(inst)),				\
		    ({}))

#define ADS124S08_SPI_CS_PTR(inst)						\
	COND_CODE_1(ADS124S08_HAS_CS(inst),				\
		    (&(ads124s08_data_##inst.cs_ctrl)),			\
		    (NULL))

#define ADS124S08_SPI_CS_LABEL(inst)					\
	COND_CODE_1(ADS124S08_HAS_CS(inst),				\
		    (DT_INST_SPI_DEV_CS_GPIOS_LABEL(inst)), (NULL))

#define ADS124S08_SPI_CFG(inst)						\
	(&(struct ads124s08_spi_cfg) {					\
		.spi_conf = {						\
			.frequency =					\
				DT_INST_PROP(inst, spi_max_frequency),	\
			.operation = (SPI_WORD_SET(8) |			\
				      SPI_OP_MODE_MASTER |		\
				      SPI_MODE_CPOL |			\
				      SPI_MODE_CPHA),			\
			.slave = DT_INST_REG_ADDR(inst),		\
			.cs = ADS124S08_SPI_CS_PTR(inst),			\
		},							\
		.cs_gpios_label = ADS124S08_SPI_CS_LABEL(inst),		\
	})

#ifdef CONFIG_ADS124S08_TRIGGER
#define GPIO_DT_SPEC_INST_GET_BY_IDX_COND(id, prop, idx)		\
	COND_CODE_1(DT_INST_PROP_HAS_IDX(id, prop, idx),		\
		    (GPIO_DT_SPEC_INST_GET_BY_IDX(id, prop, idx)),	\
		    ({.port = NULL, .pin = 0, .dt_flags = 0}))

#else
#define ADS124S08_CFG_INT(inst)
#endif /* CONFIG_ADS124S08_TRIGGER */

#define ADS124S08_CONFIG_SPI(inst)						\
	{								\
		.bus_name = DT_INST_BUS_LABEL(inst),			\
		.bus_init = ads124s08_spi_init,				\
		.bus_cfg = { .spi_cfg = ADS124S08_SPI_CFG(inst)	}, \
		ADS124S08_CFG_INT(inst)					\
	}

#define ADS124S08_DEFINE_SPI(inst)						\
	static struct ads124s08_data ads124s08_data_##inst =			\
		ADS124S08_DATA_SPI(inst);					\
	static const struct ads124s08_config ads124s08_config_##inst =	\
		ADS124S08_CONFIG_SPI(inst);				\
	ADS124S08_DEVICE_INIT(inst)

/*
 * Main instantiation macro. Use of COND_CODE_1() selects the right
 * bus-specific macro at preprocessor time.
 */

#define ADS124S08_DEFINE(inst)						\
	COND_CODE_1(DT_INST_ON_BUS(inst, spi),				\
		    (ADS124S08_DEFINE_SPI(inst)),				\
		    )

DT_INST_FOREACH_STATUS_OKAY(ADS124S08_DEFINE)

ADS124s08_SPI.c

/*
 *
 * Datasheet:
 * www.ti.com/.../ADS124S08
 */

#define DT_DRV_COMPAT ti_ads124s08

#include <string.h>
#include "ads124s08.h"
#include <logging/log.h>
#include <hal\nrf_gpio.h>



#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)

LOG_MODULE_DECLARE(ads124s08, CONFIG_SENSOR_LOG_LEVEL);

/* ADS124S08 supports only SPI mode 0, word size 8 bits, MSB first */
#define ADS124S08_SPI_CFG			SPI_WORD_SET(8)


static int ads124s08_spi_write(const struct device *dev,uint8_t value, uint8_t len)
{
	struct ads124s08_data *data = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	const struct spi_config *spi_cfg = &cfg->bus_cfg.spi_cfg->spi_conf;

	const struct spi_buf tx_buf = {
			.buf = &value,
			.len = 1,
	};
	const struct spi_buf_set tx = {
		.buffers = &tx_buf,
		.count = 1
	};

	if (len > 64) {
		return -EIO;
	}


	nrf_gpio_pin_clear(data->cs_ctrl.gpio_pin);

	if (spi_write(data->bus, spi_cfg, &tx)) {
		return -EIO;
	}

	nrf_gpio_pin_set(data->cs_ctrl.gpio_pin);

	return 0;
}


static int ads124s08_spi_read(const struct device *dev,uint8_t *value, uint8_t len)
{
	struct ads124s08_data *data = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	const struct spi_config *spi_cfg = &cfg->bus_cfg.spi_cfg->spi_conf;
	
	
	uint8_t buffer_tx[1] = {ADS124S08_CMD_NOP};

	const struct spi_buf tx_buf = {
			.buf = buffer_tx,
			.len = 1,
	};
	const struct spi_buf_set tx = {
		.buffers = &tx_buf,
		.count = 1
	};
	const struct spi_buf rx_buf[2] = {
		{
			.buf = NULL,
			.len = 2,
		},
		{
			.buf = value,
			.len = len,
		}
	};
	const struct spi_buf_set rx = {
		.buffers = rx_buf,
		.count = 2
	};


	if (len > 64) {
		return -EIO;
	}

	if (len > 1) {
		buffer_tx[0] |= 0x0;
	}

	nrf_gpio_pin_clear(data->cs_ctrl.gpio_pin);

	if (spi_transceive(data->bus, spi_cfg, &tx, &rx)) {
		return -EIO;
	}
	nrf_gpio_pin_set(data->cs_ctrl.gpio_pin);

	return 0;
}


static int ads124s08_reg_read(const struct device *dev, uint8_t reg_addr,
			    uint8_t *pRxData)
{
	struct ads124s08_data *data = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	const struct spi_config *spi_cfg = &cfg->bus_cfg.spi_cfg->spi_conf;
	const uint8_t len = 2; // read back 4 bytes from reg 


	uint8_t buffer_tx[3]; 
	buffer_tx[0] = ((ADS124S08_START_REG_MASK & reg_addr )  | ADS124S08_CMD_RREG); 
	buffer_tx[1] = 0x00; //number of registers to read minus 1 
	buffer_tx[2] = 0x00 ; // no op 

						
	const struct spi_buf tx_buf = {
			.buf = buffer_tx,
			.len = 3,
	};
	const struct spi_buf_set tx = {
		.buffers = &tx_buf,
		.count = 1
	};
	const struct spi_buf rx_buf[2] = {
		{
			.buf = NULL,
			.len = 1,
		},
		{
			.buf = pRxData,
			.len = len,
		}
	};
	const struct spi_buf_set rx = {
		.buffers = rx_buf,
		.count = 2
	};


	if (len > 64) {
		return -EIO;
	}

	if (len > 1) {
		buffer_tx[0] |= 0x0;

	}



	nrf_gpio_pin_clear(data->cs_ctrl.gpio_pin);

	if (spi_transceive(data->bus, spi_cfg, &tx, &rx)) {
		return -EIO;
	}

	nrf_gpio_pin_set(data->cs_ctrl.gpio_pin);

	return 0;
}

static int ads124s08_reg_write(const struct device *dev, uint8_t reg_addr,
			     uint8_t *value, uint8_t len)
{
	struct ads124s08_data *data = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	const struct spi_config *spi_cfg = &cfg->bus_cfg.spi_cfg->spi_conf;
	uint8_t buffer_tx[2] = { ( reg_addr & ADS124S08_START_REG_MASK) | ADS124S08_CMD_WREG , 0};
	const struct spi_buf tx_buf[2] = {
		{
			.buf = buffer_tx,
			.len = 2,
		},
		{
			.buf = value,
			.len = len,
		}
	};
	const struct spi_buf_set tx = {
		.buffers = tx_buf,
		.count = 1
	};


	if (len > 64) {
		return -EIO;
	}

	// if (len > 1) {
	// 	buffer_tx[0] |= ADS124S08_SPI_AUTOINC;
	// }

	if (spi_write(data->bus, spi_cfg, &tx)) {
		return -EIO;
	}

	return 0;
}


static int adsd124s08_read_sample(const struct device *dev, uint8_t *value, uint8_t len){ 
	return ads124s08_spi_read(dev,value,len); 	
}

static int adsd124s08_write_command(const struct device *dev, uint8_t value){ 
	return ads124s08_spi_write(dev,value,1); 	
}

static int ads124s08_spi_read_reg(const struct device *dev, uint8_t reg_addr,
				uint8_t *value)
{
	return ads124s08_reg_read(dev, reg_addr, value);

}

static int ads124s08_spi_write_reg(const struct device *dev, uint8_t reg_addr,
				uint8_t value)
{
	uint8_t tmp_val = value;

	return ads124s08_reg_write(dev, reg_addr, &tmp_val, 1);
}


static const struct ads124s08_transfer_function ads124s08_spi_transfer_fn = {
	.read_reg  = ads124s08_spi_read_reg,
	.write_reg  = ads124s08_spi_write_reg,
	.read_samp = adsd124s08_read_sample,
	.write_command = adsd124s08_write_command,
};

int ads124s08_spi_init(const struct device *dev)
{
	struct ads124s08_data *data = dev->data;
	const struct ads124s08_config *cfg = dev->config;
	const struct ads124s08_spi_cfg *spi_cfg = cfg->bus_cfg.spi_cfg;

	data->hw_tf = &ads124s08_spi_transfer_fn;

	if (spi_cfg->cs_gpios_label != NULL) {

		/* handle SPI CS thru GPIO if it is the case */
		data->cs_ctrl.gpio_dev =
			    device_get_binding(spi_cfg->cs_gpios_label);
		if (!data->cs_ctrl.gpio_dev) {
			LOG_ERR("Unable to get GPIO SPI CS device");
			return -ENODEV;
		}

		LOG_ERR("SPI GPIO CS configured on %s:%u",
			spi_cfg->cs_gpios_label, data->cs_ctrl.gpio_pin);
	}

	return 0;
}
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */

ads124s08.h

#ifndef ZEPHYR_DRIVERS_SENSOR_ADS124S08_ADS124S08_H_
#define ZEPHYR_DRIVERS_SENSOR_ADS124S08_ADS124S08_H_


#include <kernel.h>
#include <device.h>
#include <sys/util.h>
#include <stdint.h>
#include <drivers/gpio.h>
#include <drivers/sensor.h>
#include <string.h>


#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
#include <drivers/spi.h>
#endif


#define DEBUG_MODE (1)
#if(DEBUG_MODE)
	#define DEBUG_PRINT printk 
#else
	#define DEBUG_PRINT(...)
#endif

#define HIGH (0xFF)
#define LOW  (0x00)


#define MULTI_CHANNEL_READ (0) // read through every channel 
 
#define ENABLE_SOFT_CONFIGS (0)

// #define SINGLE_SHOT_MODE

#if defined(SINGLE_SHOT_MODE)
	#define SINGLE_SHOT_MODE_BIT (0x20)
#else 
	#define SINGLE_SHOT_MODE_BIT (0x00)
#endif
// GPIO Pins

// #define ADS124S08_CS_LABEL	      DT_GPIO_LABEL(DT_ALIAS(gpiocus0), gpios)
// #define ADS124S08_CS_PIN	      DT_GPIO_PIN(DT_ALIAS(gpiocus0), gpios)
#define ADS124S08_RESET_LABEL 	  DT_GPIO_LABEL(DT_ALIAS(gpiocus1), gpios)
#define ADS124S08_RESET_PIN	      DT_GPIO_PIN(DT_ALIAS(gpiocus1), gpios)
#define ADS124S08_START_LABEL     DT_GPIO_LABEL(DT_ALIAS(gpiocus2), gpios)
#define ADS124S08_START_PIN	      DT_GPIO_PIN(DT_ALIAS(gpiocus2), gpios)


// Interrupt Pins
#if DT_INST_PROP_HAS_IDX(0, irq_gpios, 1)
/* INT1 is configured */
#define ADS124S08_INT1_GPIOS_PIN		DT_INST_GPIO_PIN_BY_IDX(0, irq_gpios, 0)
#define ADS124S08_INT1_GPIOS_FLAGS		DT_INST_GPIO_FLAGS_BY_IDX(0, irq_gpios, 0)
#define ADS124S08_INT1_GPIO_DEV_NAME	DT_INST_GPIO_LABEL_BY_IDX(0, irq_gpios, 0)
#else

#define ADS124S08_INT1_GPIOS_PIN		DT_INST_GPIO_PIN(0, irq_gpios)
#define ADS124S08_INT1_GPIOS_FLAGS		DT_INST_GPIO_FLAGS(0, irq_gpios)
#define ADS124S08_INT1_GPIO_DEV_NAME	DT_INST_GPIO_LABEL(0, irq_gpios)

#endif


#define DRDY_PIN (43)

#define RES (double)((double)VREF/pow(2,23))

// Commands 

#define ADS124S08_CMD_NOP	0x00
#define ADS124S08_CMD_WAKEUP	0x02
#define ADS124S08_CMD_PWRDWN	0x04
#define ADS124S08_CMD_RESET	0x06
#define ADS124S08_CMD_START	0x08
#define ADS124S08_CMD_STOP	0x0A
#define ADS124S08_CMD_SYOCAL	0x16
#define ADS124S08_CMD_SYGCAL	0x17
#define ADS124S08_CMD_SFOCAL	0x19
#define ADS124S08_CMD_RDATA	0x12
#define ADS124S08_CMD_RREG	0x20
#define ADS124S08_CMD_WREG	0x40

// Registers 

#define ADS124S08_REG_ID 0x00
#define ADS124S08_REG_STATUS 0x01
#define ADS124S08_REG_INPMUX 0x02
#define ADS124S08_REG_PGA 0x03
#define ADS124S08_REG_DATARATE 0x04
#define ADS124S08_REG_REF 0x05
#define ADS124S08_REG_IDACMAG 0x06
#define ADS124S08_REG_IDACMUX 0x07
#define ADS124S08_REG_VBIAS 0x08
#define ADS124S08_REG_SYS 0x09
#define ADS124S08_REG_OFCAL0 0x0A
#define ADS124S08_REG_OFCAL1 0x0B
#define ADS124S08_REG_OFCAL2 0x0C
#define ADS124S08_REG_FSCAL0 0x0D
#define ADS124S08_REG_FSCAL1 0x0E
#define ADS124S08_REG_FSCAL2 0x0F
#define ADS124S08_REG_GPIODAT 0x10
#define ADS124S08_REG_GPIOCON 0x11


/* ADS124S0x common channels */
#define ADS124S08_AIN0		0x00
#define ADS124S08_AIN1		0x01
#define ADS124S08_AIN2		0x02
#define ADS124S08_AIN3		0x03
#define ADS124S08_AIN4		0x04
#define ADS124S08_AIN5		0x05
#define ADS124S08_AINCOM	0x0c
#define ADS124S08_AIN6		0x06
#define ADS124S08_AIN7		0x07
#define ADS124S08_AIN8		0x08
#define ADS124S08_AIN9		0x09
#define ADS124S08_AIN10		0x0a
#define ADS124S08_AIN11		0x0b
#define ADS124S08_MAX_CHANNELS	12

#define ADS124S08_POS_MUX_SHIFT	0x04
#define ADS124S08_INT_REF		0x09

#define ADS124S08_START_REG_MASK	0x1f
#define ADS124S08_NUM_BYTES_MASK	0x1f

#define ADS124S08_START_CONV	0x01
#define ADS124S08_STOP_CONV	0x00


#define ADS124S08_CHIP_ID 0x00 

#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
struct ads124s08_spi_cfg {
	struct spi_config spi_conf;
	const char *cs_gpios_label;
};
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */

union ads124s08_bus_cfg {

#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
	const struct ads124s08_spi_cfg *spi_cfg;
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */
};

struct ads124s08_config {
	const char *bus_name;
	int (*bus_init)(const struct device *dev);
	const union ads124s08_bus_cfg bus_cfg;
};

struct ads124s08_transfer_function {
	int (*read_reg)(const struct device *dev, uint8_t reg_addr,
			uint8_t *value);
	int (*write_reg)(const struct device *dev, uint8_t reg_addr,
			 uint8_t value);
	int (*read_samp)(const struct device *dev, uint8_t *value, uint8_t len);
	int (*write_command)(const struct device *dev, uint8_t value);

};


union asd124s08_sample{ 
	uint8_t bytes[3];  
	uint32_t raw[1]; 
}; 

struct ads124s08_data {
	const struct device *bus;
	const struct ads124s08_transfer_function *hw_tf;
	union asd124s08_sample sample;
	uint8_t tempRecordings[18]; // 3 bytes per sample * 6 channels = 18 bytes

#ifdef CONFIG_ADS124S08_TRIGGER
	const struct device *dev;
	const struct device *gpio_int1; 
	struct gpio_callback gpio_int1_cb;
	
	sensor_trigger_handler_t handler_drdy;
	atomic_t trig_flags;
	enum sensor_channel chan_drdy;

#if defined(CONFIG_ADS124S08_TRIGGER_OWN_THREAD)
	K_KERNEL_STACK_MEMBER(thread_stack, CONFIG_ADS124S08_THREAD_STACK_SIZE);
	struct k_thread thread;
	struct k_sem gpio_sem;
#elif defined(CONFIG_ADS124S08_TRIGGER_GLOBAL_THREAD)
	struct k_work work;
#endif

#endif /* CONFIG_ADS124S08_TRIGGER */

#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
	struct spi_cs_control cs_ctrl;
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */
};


#ifdef CONFIG_ADS124S08_TRIGGER
int ads124s08_trigger_set(const struct device *dev,
		       const struct sensor_trigger *trig,
		       sensor_trigger_handler_t handler);

int ads124s08_init_interrupt(const struct device *dev);

#endif

int ads124s08_spi_init(const struct device *dev);

#endif 

覆盖文件:  

/*
 * Copyright (c) 2019 Nordic Semiconductor ASA
 *
 * SPDX-License-Identifier: Apache-2.0
 */

 &spi2 {
	compatible = "nordic,nrf-spim";
	status = "okay";
	sck-pin = <47>;
	mosi-pin = <45>;
	miso-pin = <46>;
	cs-gpios = <&gpio1 12 GPIO_ACTIVE_LOW>;

	ads124s08@0 {
		compatible = "ti,ads124s08";
		label = "ADS124S08";
		spi-max-frequency = <5000000>;
		reg = <0>;
		irq-gpios = <&gpio1 11 GPIO_ACTIVE_LOW>;
		
	};
};


&uart0 {
	status = "okay";
	current-speed = <115200>;
	tx-pin = <20>;
	rx-pin = <22>;
	rts-pin = <19>;
	cts-pin = <21>;
};

/ {
    gpiocustom {
        compatible = "gpio-keys";
        // gpiocus0: gpiocus_0 {
        //     gpios = <&gpio1 12 GPIO_ACTIVE_LOW>;
        //     label = "CS";
        // };
        gpiocus1: gpiocus_1 {
            gpios = <&gpio1 10 GPIO_ACTIVE_LOW>;
            label = "RESET";
        };

		gpiocus2: gpiocus_2 {
            gpios = <&gpio0 27 GPIO_ACTIVE_HIGH>;
            label = "START";
        };
    };
    aliases {
        // gpiocus0 = &gpiocus0;
        gpiocus1 = &gpiocus1;
		gpiocus2 = &gpiocus2;

    };
};

如有任何帮助,我们将不胜感激。  

谢谢!  

马特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Matt,您好!

    您是否在GitHub上看到了Linux驱动程序:

    https://github.com/torvalds/linux/blob/master/drivers/iio/adc/ti-ads124s08.c

    有几件事需要检查。  第一个AVDD/AVSS,DVDD和IOVDD必须全部处于额定工作电压。  如果缺少电源(例如模拟电源),ADS124S08将保持在重置状态。  接下来,检查复位销是否拉高。  在沟通过程中,检查沟通过程中的阶段是否正确。  我无法从逻辑分析器镜头判断,但数据应在SCLK的上升沿上发生变化,并在下降沿上保持稳定。

    此致,

    Bob B

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bob,您好!  

    感谢您的回复。

    我已确认以下事项:  

    AVDD:5V

    IOVDD3.3V

    DVDD:3.3V

    以下是显示重置引脚的波形:  

    我可以在固件中将其切换为高和低,这样我就不认为 它一定处于重置状态。  

    是的,我遇到了这个驱动程序,我使用的是基于 Linux的Zephyr RTOS。 它与您提供的代码相似,正如您所看到的,我的实现 有点 相似。  

    感谢您的帮助,  

    马特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Matt,您好!

    您使用的是Saleae。  是否可以导出并附加.Sal文件?  如果不可能,您能否向我发送一个更缩放的版本,以便我验证通信内容?

    谢谢!

    Bob B

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bob,您好!  

    请参阅随附的.Sal文件。  

    谢谢!  

    马特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Matt,您好!

    我本来应该在开始时更清楚一点。  您需要确保您的SCLK时钟停留在较低和较高的位置。  您的阶段也不正确。  确保遵循数据表SPI规范。

    此致,

    Bob B

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bob,您好!  

    我将CPOL更改为0 ,将CPHA更改为1,以产生以下波形。 相位和极性似乎正确。 但寄存器仍在读取零。 有什么想法吗?  

    谢谢!  

    马特  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Matt,您好!

    RREG命令为2个字节。  您正在显示正在发出RREG (0x20)命令以从寄存器4开始(第一个字节的命令总数为0x24),只读取一个寄存器(命令的第二个字节为0x00),返回值不是0x00而是0x14。  0x14是寄存器0x04的默认值。

    因此逻辑数据是正确的。  您可能没有在代码中捕获正确的字节。

    此致,

    Bob B