This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS805:将与配合使用

Guru**** 2925550 points

Other Parts Discussed in Thread: ADS805

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/579563/ads805-will-work-with-a

部件号:ADS805

如果我提供来自函数发生器的3Vp-p正弦波输入信号,则输出将参考共模电压或0伏???

我已将ADS805连接为附加图像文件。

谢谢

Eashwar

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Eashwar,

    如果您的输入为0 - 3V,则需要提供1V的参考电压,将ADC设置为外部参考电压模式,并将1.5V提供给输入电压。 这将通过输入中的0-3V输入为您提供平衡输出。 请参见ADS805数据表第11页上的图10。 如果将所示电路用于0-3V输入,则一旦输入超过0.5V,您将进行剪辑。

    此致,

    Jim