This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1299:Ads1299不工作Vcap1出现-1.1V

Guru**** 2581345 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/579252/ads1299-ads1299-doesnt-work-vcap1-appear--1-1v

部件号:ADS1299

我正在使用openbci电路并插入5V

我的LDO稳压器使3V DVDD和2.5V AVDD - 2.5 可用

但当我看到数据表时,VCAP1显示为- 1.1 ,当我开始开机并重置时,数据表会显示。 我必须等待高于1.1 V的VCAP1

但我的电路VCAP1为-1.1V (负)

所以我不知道为什么……请帮我