This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] RCV420:RCV420 ADC值不稳定

Guru**** 2943400 points

Other Parts Discussed in Thread: RCV420

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/587421/rcv420-rcv420-adc-value-not-stable

部件号:RCV420
主题中讨论的其他部件:TM4C123

您好,  

我有一个高精度压力传感器,其输出为4-20mA。 我使用了RCV420将电流转换为 0到3.3V电压,这是提供给TM4C123启动板的。  

问题是CCS上显示的ADC值不是稳定值。 每当我通过RCV420将压力传感器连接到启动板时,该值会在实际值的+或- 10之间波动。  

我已将RCV420电路的连接连接连接到通用板上。  

我已将RCVout连接到启动板ADC引脚。 电阻器R8和R9的值设置为137欧姆。  

如何稳定ADC值??

此致

Praveen