请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS1293 大家好,
我们希望将ADS1293引脚的SYNCB引脚用作同步输入, 以便使ADS1293与加速计同步。
计划将我们的微控制器用作ADS1293和加速计的SyncGenerator。
ADS1293配置:
-1个通道
- ODR = 400Hz
是否有人可以确认是否可以使用SYNCB进行外部同步?
此致,
Rene
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好Rene:
Brian