请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:TVP7002不建议在新设计中使用TVP7002芯片TI网站,建议使用类似VGA信号的AD芯片。
对于:
像素速率高达165 MHz
只设计带有VGA信号的广告
支持RGS至YCbCr颜色空间转换,YCbCr 4:2:2输出
以上,请推荐备用信号,紧急,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.