This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS4449EVM:帮助您选择&'ads4449'

Guru**** 2966500 points

Other Parts Discussed in Thread: ADS4449, ADS58H40

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/621586/ads4449evm-help-for-choosing-voltage-supply-source-for-ads4449

部件号:ADS4449EVM
主题中讨论的其他部件:ADS4449, ADS58H40

我想使用'ADS4449'来操作我们系统的AD转换。
根据数据表,芯片有3个电压电源:3.3V,1.9V和1.8V。
但是,在'ADS4449 EVM(ADS58H40 EVM)'的原理图中,只使用了2个电压源,即3.3V和1.9V。
当我只使用2个电压源时,电路是否正常工作?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Youngho,

    根据数据表,这两种电源的使用电压最高可达2V,因此这应该不是问题。

    此致,

    Jim