请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS1675 大家好,
读取ADS1675 I的数据表时,上升/下降时间为1ns。 我找不到能够处理上升/下降时间的振荡器。 有人可以提出建议吗?
在参考设计上,有一个clk信号通过OR-Gate从FPGA进入ADS1675。 但是,该OR-Gate也不能处理上升/下降时间。
有人能帮我吗?
谢谢!
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.