请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TSW14J56EVM 您好,我正在使用TSW14J56EVM板,想知道可以发送到该板的文件大小有何限制?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我正在使用TSW14J56EVM板,想知道可以发送到该板的文件大小有何限制?
您好,Dillon:
TSW14J56具有4x8Gb DDR3内存。 这转换为32G的存储。 或2G的16位样本。
我认为内存被拆分为TX和RX内存,因此您应该能够加载包含1Gsamplesof data的文件。 尽管这是可能的,但由于PC系统的限制以及从PC到TSW14J56 EVM的传输速度,这可能并不实际。
我们使用的大多数大文件通常是10ms的数据帧-这可能是10-20M以上的样本。
肯