大家好,
在ads1299中,PGA被指定为1,2,4, 6,8,12,24 ...选择以下增益时,什么是触觉??因为这个领域的新情况是,这个PGA设置让我挣扎了很多...我需要知道当选择增益值时,这背后发生了什么...因为EEG信号需要成千上万的增益,这里的增益是24 I AM 对工作感到困惑...大家会详细解释一下...提前感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
在ads1299中,PGA被指定为1,2,4, 6,8,12,24 ...选择以下增益时,什么是触觉??因为这个领域的新情况是,这个PGA设置让我挣扎了很多...我需要知道当选择增益值时,这背后发生了什么...因为EEG信号需要成千上万的增益,这里的增益是24 I AM 对工作感到困惑...大家会详细解释一下...提前感谢
您好,LF:
请参阅用户指南第51页的示意图。 J6上安装了一系列并联跳线,它们馈入ADS1299的AINxN和AINxP引脚。 拆下与AINxP信号相对应的分流器,这些分流器将穿过针脚7-8,11-12等向下穿过针脚35-36。 将分流跳线放在JP-25的引脚1-2和5-6之间。 从这里,您的信号发生器参考(GND)可以连接到TP12。 信号发生器输出可通过引脚36应用到J6引脚8,12,16等。
先生,我尝试了一些输入...我使用CRO和函数发生器将Vpp设置为1V,将频率设置为80.7 Hz ... ADS1299 EEG-FE套件中的设置如下所示
1.使用单端输入
2. 从J6的32-36上卸下跳线,将函数发生器的正极连接到J6的引脚36,将GROUND连接到J6的引脚34。
3. 将SRB1位设置为关闭
4. 将PGA增益设置为1
5.使用正弦波作为输入进行检查
但我没有得到预期的正弦波...我有一些其他waveform...plz解释了我的问题...设置或连接?让我在下面发布图片...