请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DAC3482 我正在开发一种在DAC3482的TXENABLE引脚上具有上拉电阻的设计。 这基本上总是启用DAC。 如果我在config3中启用/禁用带有sif_txenable位的DAC,这是否会覆盖基于TXEANBLE引脚的设置,还是因为引脚被拉高而始终启用DAC?
谢谢!
标记
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.