请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS8684 亲爱的戴尔:
我的客户在用ADS8684的时候由于前级输入信号有一些干扰,所以在输入的这里加入了RC滤波滤掉信号噪声。如图所示,R = 20k,C = 0.01uF。 但是这样的配置导致增益有偏差,之前增益设定为1,加入RC滤波增益偏移20 %。请问这种情况下如何通过读数来补偿这种增益偏移带来的误差从而回归到读取出真实值?
感谢您的答复!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.