This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DAC2904:输出符合性

Guru**** 2927270 points

Other Parts Discussed in Thread: DAC2904

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/597365/dac2904-output-compliance

部件号:DAC2904

我们在 新设计中使用DAC2904,并且对其中一个规格有疑问。  根据
在数据表的第3页,输出符合性范围是-1.0V到+1.25V,但这是在时间
VA=+5V。  数据表的下一页3显示了电压范围为+3.0V至+5.5V的电压。

使用VA=+3.3V操作DAC2904将如何影响输出符合范围?

非常感谢