我正在使用TI的TVP5158,它正在调试中
以下问题:设置为CH1,A/D,VO_A以输出8位的D1信号,
但后者不被承认。 原因是什么?接下来我应该怎么做?非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!底部是TVP5158的寄存器设置,工作模式
它是模拟CVBS输入通道1,PAL信号,输出选择DVO_1,
格式为8位DI格式,但转换芯片无法识别后者。
接收到标准DI信号,芯片输入端口为正常。
寄存器设置:
信号链路:
CVBS输入-------- TVP5158 --- FPGA --- GS2972
1.当前状态:
将TVP5158设置为单模式,GS2972无法检测到输出信号。
TVP5158输出时钟:27m;
TVP5S的DVD_A输出数据输入了FPGA提取HS。
但当您消除输入CVBS时,HS,VS和OE是正常的;
其他测试:FPGA使用TVP5158的27M时钟输出生成色条测试图,GS2972检测到该值。
输出正常显示。
二.
TVP5158套件内容:
在DVD_A处输出TVP5a自身的蓝场测试信号
格式:8bit d1 format.PAL系统。
TVP5158寄存器如下所示:
00h:7E b0 03 00 02 00 00 51 58 71 02 82 00 ff 03
10小时:80 00 80 00 00 70 0A 40 00 00 00 0 c 00 00 00 00 00
20h:6a 08 80 80 00 F5 00 00 00 00 06 1e 04 00 f2 08 04
30小时:FF ff ff 00 00 6a 08 05 07 84 00 d0 02 19 00 20 01
40小时:07 00 47 00 04 00 07 00 84 00 d0 02 6F 02 18 00
50小时:84 00 d0 02 97 00 bc 02 26 00 06 01 1e 09 34 03
60H:00 09 40 1e 18 00 0b 00 1f 1f 02 10 04 64 20
70小时:7D 00 8a 64 04 02 0f 0f 03 05 20 1e 02 08 03
80h:0A 01 5a 06 00 03 22 00 00 12 1D 64 00 0A 04
90小时:10 80 80 00 4c 1a 60 50 00 00 00 0A 05 05 03 bc.
A0H:BC 00 0d 02 90 01 78 00 08 03 D8 05 00 01 00
B0H:00 ff ff E4 00 71 12 40 00 01 D7 0f 00 00
C0H:00 88 C9 01 00 00 00 00 00 A5 ff 7e 01 00 00 00 00
D0H:00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
E0H:00 00 00 00 25 25 25 25 54 00 00 00 00 00 00 00 0025.
F0h:08 00 00 00 00 00 00 00 00 00 25 25 25 25 25 2f 01
3.
在VIN_1中输入CVBS (PAL颜色条)
该寄存器与上一个寄存器相同,但A9:40。