主题中讨论的其他部件: ADS124S08
您好,
在将ADS124S08EVM的AIN2和AIN4终端修改为与外部Linux处理器配合使用后,IVE将K型热电偶连接到了AIN2和AIN4终端。 参见以下规格。
我对ASD124S08 EVM https://www.ti.com/tool/ADS124S08EVM上的JP1进行了短接 ,以便可以使用另一个微控制器对其进行控制。
微控制器: nrf5340-dk
RTOS:Zephyr.
SDK:nrf SDK 1.8 .........0
SPI时钟:5MHz
IVE遵循 了《热电偶测量基本指南 》中的说明,产生的原始计数似乎非常高。 我将指南中的公式应用于原始计数,我看到电压记录的值非常高。,
请参阅下面的寄存器配置。
注册地图:
00>[00:00:00。ADS]<INF> ads124s08:55.13万 124S08检测到ID:8
00>[00:00:00.ad] 55.2062万 <inf> ads124s08:reg: 0,val 8.
00>[00:00:00:00.ad] 55.2124万 <inf> ads124s08:reg: 1, val 80
00>[00:00:00.ad] 55.2185万 <inf> ads124s08:reg: 2,val 24.
00>[00:00:00.ad] 55.2276万 <inf> ads124s08:reg: 3,val 2.
00>[00:00:00.ad] 55.2337万 <inf> ads124s08:reg: 4,val 14.
00>[00:00:00.ad] 55.2429万 <inf> ads124s08:reg: 5,val 10.
00>[00:00:00.ad] 55.249万 <inf> ads124s08:reg: 6,val 0
00>[00:00:00.ad] 55.2581万 <inf> ads124s08:reg: 7,val ff
00>[00:00:00.ad] 55.2642万 <inf> ads124s08:reg: 8,val 10.
00>[00:00:00.ad] 55.2734万 <inf> ads124s08:reg: 9,val 10.
00>[00:00:00.ad] 55.2795万 <inf> ads124s08:reg: a,val 0
00>[00:00:00.ad] 55.2856万 <inf> ads124s08:reg: b , val 0
00>[00:00:00.ad] 55.2947万 <inf> ads124s08:reg: c,val 0
00>[00:00:00.ad] 55.3009万 <inf> ads124s08:reg: d,val 0
00>[00:00:00.ad] 55.307万 <inf> ads124s08:reg: e,val 0
00>[00:00:00.ad] 55.3161万 <inf> ads124s08:reg: F,val 40.
00>[00:00:00.ad] 55.3222万 <inf> ads124s08:reg: 10,val 0
00>[00:00:00.ad] 55.3283万 <inf> ads124s08:reg: 11,val 0
输出:(时间戳,原始计数,样品和转换电压(应用指南中的公式3):
00>[00:01:17.mV] 84.1857万 <inf> ads124s08:原始:FF,ff,96,样本:1677.711万,电压319mV
00>[00:01:17.mV] 90.8721万 <inf> ads124s08:原始:FF,ff,99,样本:1677.7113万,电压319mV
00>[00:01:17.mV]<inf> ads124s08:原始:97.5585万 ,ff,9d,样品:1677.7117万,电压319mV
00>[00:01:18.mV] 4.2449万 <inf> ads124s08:原始:FF,ff,98,样本:1677.7112万,电压319mV
00>[00:01:18.mV]<inf> ads124s08:原始:10.9313万 ,ff,99,样品:1677.7113万,电压319mV
00>[00:01:18.mV] 17.6177万 <inf> ads124s08:原始:FF,ff,96,样本:1677.711万,电压319mV
00>[00:01:18.mV] 24.3041万 <inf> ads124s08:原始:FF,ff,96,样本:1677.711万,电压319mV
00>[00:01:18.mV]<inf> ads124s08:原始:30.9906万 ,ff,9a,样品:1677.7114万,电压319mV
00>[00:01:18.mV] 37.677万 <inf> ads124s08:原始:FF,ff,98,样本:1677.7112万,电压319mV
00>[00:01:18.mV] 44.3634万 <inf> ads124s08:原始:FF,ff,97,样本:1677.7111万,电压319mV
00>[00:01:18.mV]<inf> ads124s08:原始:51.0528万 ,ff,9c,样品:1677.7116万,电压319mV
00>[00:01:18.mV] 57.7392万 <inf> ads124s08:原始:FF,ff,98,样本:1677.7112万,电压319mV
00>[00:01:18.mV] 64.4256万 <inf> ads124s08:原始:FF,ff,98,样本:1677.7112万,电压319mV
发送RDATA命令时,请参阅逻辑分析器的以下屏幕截图:

请参阅下面的ADS124S08.c代码:
#define DT_DRV_COMPAT ti_ads124s08
#include <init.h>
#include <sys/byteorder.h>
#include <sys/__assert.h>
#include <logging/log.h>
LOG_MODULE_REGISTER(ads124s08, CONFIG_SENSOR_LOG_LEVEL);
#include "ads124s08.h"
#include <devicetree.h>
#include <drivers/gpio.h>
#include <nrf.h>
#include <hal/nrf_gpio.h>
static const struct device *dev_start;
static const struct device *dev_reset;
static int ads124s08_reg_readout(const struct device *dev);
// configure GPIO Pins for CS, Start and reset
static void init_gpio(void) {
int status;
dev_reset = device_get_binding(ADS124S08_RESET_LABEL);
if (dev_reset == NULL){
LOG_ERR("dev_reset device_get_binding() failure.");
return;
}
status = gpio_pin_configure(dev_reset, ADS124S08_RESET_PIN, GPIO_OUTPUT_ACTIVE);
if (status < 0){
LOG_ERR("dev_reset gpio_pin_configure() failure.");
return;
}
dev_start= device_get_binding(ADS124S08_START_LABEL);
if (dev_start == NULL){
LOG_ERR("dev_start device_get_binding() failure.");
return;
}
status = gpio_pin_configure(dev_start, ADS124S08_START_PIN, GPIO_OUTPUT_ACTIVE);
if (status < 0){
LOG_ERR("dev_start gpio_pin_configure() failure.");
return;
}
#ifndef CONFIG_ADS124S08_TRIGGER
nrf_gpio_cfg_input(DRDY_PIN, NRF_GPIO_PIN_PULLUP);
#endif
}
static void ads124s08_set_start_pin(int STATE){
gpio_pin_set(dev_start, ADS124S08_START_PIN, STATE);
}
static void ads124s08_set_reset_pin(int STATE){
gpio_pin_set(dev_reset, ADS124S08_RESET_PIN, STATE);
}
/*
Write ADC Values to Sensors Val Stict
*/
static int ads124s08_channel_get(const struct device *dev,
enum sensor_channel chan,
struct sensor_value *val)
{
struct ads124s08_data *ads124s08 = dev->data;
val->pData = ads124s08->sample.bytes;
return 0;
}
/*
Convert internal temperate readings
*/
static void convert_internal_temp(const struct device *dev, uint32_t samp){
struct ads124s08_data *ads124s08 = dev->data;
double scaleFactor = (double)((VREF) / (ADS124S08_PGA_FACTOR * 8388608));
double voltage = scaleFactor * (double)samp;
ads124s08->cjv = voltage;
ads124s08->tempCj = (((voltage - 129) / 403 )) + 25;
}
/*
Convert internal temperate readings
*/
static void convert_themocouple_temp(const struct device *dev, uint32_t samp){
struct ads124s08_data *ads124s08 = dev->data;
double scaleFactor = (double)((VREF) / (ADS124S08_PGA_FACTOR * 32768));
double voltage = scaleFactor * (double)samp ;
ads124s08->chanV = voltage;
}
/*
Read data from ADC Channels
*/
static uint32_t ads124s08_read_data(const struct device *dev){
struct ads124s08_data *ads124s08 = dev->data;
int status;
uint32_t samp;
uint8_t sample[RDATA_CMD_READ_BACK_LEN];
status = ads124s08->hw_tf->read_samp(dev,&sample[0]); //send RDATA Command
if(status < 0){
LOG_ERR("Error. asd124s08_read_data(). Unable to fetch sample" );
return 1;
}
samp = (uint32_t)(sample[0] << 16 | sample[1] << 8 | sample[2]);
// record internal temp on every other interval
if (ads124s08->internalTempSetBit > 0 ){
convert_internal_temp(dev, samp);
}else{
convert_themocouple_temp(dev, samp);
#if !(MODE_CHANNEL_READ_ONLY)
if (ads124s08->cjv >0){
DEBUG_LOG("ChanV: %dmV, Internal V:%dmV, CJT:%d C, V + VCJ: %dmV ", ads124s08->chanV,ads124s08->cjv,ads124s08->tempCj , ads124s08->chanV + ads124s08->cjv);
}
#else
DEBUG_LOG("Raw: %x, %x, %x , Sample: %d, Voltage %dmV ", sample[0],sample[1], sample[2], samp, ads124s08->chanV );
#endif
}
return 0;
}
/*
When measuring the internal temperature sensor, the analog inputs are disconnected from the ADC and the
output voltage of the temperature sensor is routed to the ADC for measurement using the selected PGA gain,
data rate, and voltage reference. If enabled, PGA gain must be limited to 4 for the temperature sensor
measurement to remain within the allowed absolute input voltage range of the PGA. As a result of the low device
junction-to-PCB thermal resistance (RθJB), the internal device temperature closely tracks the printed circuit board
(PCB) temperature.
*/
static int ads124s08_toggle_internal_temp_settings(const struct device *dev){
struct ads124s08_data *ads124s08 = dev->data;
static uint8_t ctrl;
static uint8_t status;
k_sleep(K_MSEC(5));
// Write ref Reg
ads124s08->internalTempSetBit ^= 0x1A; // measures internal temp every other interupt
ctrl = 0x10 | ads124s08->internalTempSetBit;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_REF, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
status = ads124s08->hw_tf->read_reg(dev,ADS124S08_REG_SYS, &ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
ctrl ^= 0x40; //toggle the internal sensor reading
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_SYS, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
status = ads124s08->hw_tf->read_reg(dev,ADS124S08_REG_PGA, &ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
ctrl ^= 0x0A; // Enable PGA and set gain to 4
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_PGA, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
return 0;//ads124s08_reg_readout(dev);
}
static int ads124s08_sample_fetch(const struct device *dev,
enum sensor_channel chan)
{
struct ads124s08_data *ads124s08 = dev->data;
uint32_t sample;
#ifndef CONFIG_ADS124S08_TRIGGER
ads124s08->drdyPinStatus = nrf_gpio_pin_read(DRDY_PIN);
if (ads124s08->drdyPinStatus == LOW){
while (!nrf_gpio_pin_read(DRDY_PIN)){
sample = ads124s08_read_data(dev); // read data from ADC
}
ads124s08->hw_tf->write_command(dev,ADS124S08_CMD_STOP );
k_sleep(K_MSEC(5));
#if !(MODE_CHANNEL_READ_ONLY)
ads124s08_toggle_internal_temp_settings(dev);
#endif
k_sleep(K_MSEC(5));
ads124s08->hw_tf->write_command(dev,ADS124S08_CMD_START );
k_sleep(K_MSEC(5));
}
#else
sample = ads124s08_read_data(dev); // read data from ADC
k_sleep(K_MSEC(5));
// ads124s08_set_internal_temp(dev); // switch to monitor internal temp
#endif
return 0;
}
static const struct sensor_driver_api ads124s08_driver_api = {
#if CONFIG_ADS124S08_TRIGGER
.trigger_set = ads124s08_trigger_set,
#endif
.sample_fetch = ads124s08_sample_fetch,
.channel_get = ads124s08_channel_get,
};
static int ads124s08_reg_readout(const struct device *dev){
struct ads124s08_data *ads124s08 = dev->data;
uint8_t status;
static uint8_t value;
for ( int i =0; i < 18; i ++){
status = ads124s08->hw_tf->read_reg(dev, i, &value);
if (status < 0){
LOG_ERR("ads124s08_reg_readout. Unable to read reg: %x", i);
}
DEBUG_LOG("REG: %x , val %x", i, value);
}
}
static int ads124s08_reset(const struct device *dev){
#if ENABLE_SOFT_CONFIGS // software reset
struct ads124s08_data *ads124s08 = dev->data;
ctrl = ADS124S08_CMD_RESET;
int status = ads124s08->hw_tf->write_command(dev, ctrl);
if (status < 0){
LOG_ERR("ads124s08_reset(). Unable to write reset command ");
}
#else // hardware reset
ads124s08_set_reset_pin(HIGH);
k_sleep(K_MSEC(100));
ads124s08_set_reset_pin(LOW);
k_sleep(K_MSEC(100));
ads124s08_set_reset_pin(HIGH);
k_sleep(K_MSEC(100));
#endif
return 0;
}
static int ads124s08_wreg_config(const struct device *dev){
struct ads124s08_data *ads124s08 = dev->data;
uint8_t ctrl;
int status;
// send wreg command to enable register writting
// write ID Reg -
ctrl = 0x08;
status = ads124s08->hw_tf->write_reg(dev, ADS124S08_REG_ID,ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write ID Reg.\n");
return status;
}
// // write Status Reg
ctrl = 0x80;
status = ads124s08->hw_tf->write_reg(dev, ADS124S08_REG_STATUS,ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write ID Reg.\n");
return status;
}
// write MUX Reg set channel 2 as positive channel 4 as negative
ctrl = 0x20 | 0x04;
status = ads124s08->hw_tf->write_reg(dev, ADS124S08_REG_INPMUX,ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write MUX Reg.\n");
return status;
}
// Write PGA Reg (cannot exceed gain of 4 or bit reg of (0x02) for internal temp readings)
ctrl = 0x00 | ADS124S08_PGA_IDX;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_PGA, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write PGA Reg.\n");
return status;
}
// Write data rate Reg
ctrl = 0x14 | SINGLE_SHOT_MODE_BIT;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_DATARATE, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write data rate Reg.\n");
return status;
}
// Write ref Reg
ctrl = 0x10;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_REF, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write Ref Reg.\n");
return status;
}
// Write IDACMAG Reg
ctrl = 0x00;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_IDACMAG, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write IDACMAG Reg.\n");
return status;
}
// Write IDACMUX Reg
ctrl = 0xFF;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_IDACMUX, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write IDACMUX Reg.\n");
return status;
}
// Write ADS124S08_REG_SYS *4 bit samples, enable crc and send stat)
ctrl = 0x10 ;// | 0x02 | 0x01;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_SYS, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write IDACMUX Reg.\n");
return status;
}
// Write ADS124S08_REG_VBIAS For Thermocouples (Vbias AIN4 for now)
ctrl = 0x00 | 0x10;
status = ads124s08->hw_tf->write_reg(dev,ADS124S08_REG_VBIAS, ctrl);
if (status < 0) {
LOG_ERR("ads124s08_wreg_config(): Failed to write IDACMUX Reg.\n");
return status;
}
#ifdef CONFIG_ADS124S08_TRIGGER
status = ads124s08_init_interrupt(dev);
if (status < 0) {
LOG_ERR("Failed to initialize interrupts.");
return status;
}
#endif
return ads124s08_reg_readout(dev);
}
static int ads124s08_init(const struct device *dev)
{
struct ads124s08_data *ads124s08 = dev->data;
const struct ads124s08_config *cfg = dev->config;
int status;
uint8_t id;
ads124s08->bus = device_get_binding(cfg->bus_name);
if (!ads124s08->bus) {
LOG_ERR("master not found: %s", cfg->bus_name);
return -EINVAL;
}
cfg->bus_init(dev);
init_gpio();
//Reset Device
status = ads124s08_reset(dev);
if (status < 0){
LOG_ERR("ads124s08_init(). Unable to reset device");
}
status = ads124s08->hw_tf->read_reg(dev, ADS124S08_REG_ID, &id);
if (status < 0)
{
LOG_ERR("ads124s08_init. Unable to read reg: %x", ADS124S08_REG_ID);
}
else if (id != ADS124S08_CHIP_ID )
{
DEBUG_LOG("Unknown device with ID %x Detected on SPI bus", id);
}
else
{
DEBUG_LOG("ADS124S08 Detected with ID: %x",id);
}
#if(INTERNAL_TEMP_TEST)
ads124s08_toggle_internal_temp_settings(dev);
#else
//config production registers
status = ads124s08_wreg_config(dev);
if ( status < 0){
LOG_ERR("ads124s08_init(). Unable to write config registers");
}
#endif
#if (HW_START)
// toggle start pin
ads124s08_set_start_pin(HIGH);
k_sleep(K_MSEC(10));
ads124s08_set_start_pin(LOW);
k_sleep(K_MSEC(10));
ads124s08_set_start_pin(HIGH);
#else
ads124s08_set_start_pin(LOW);
k_sleep(K_MSEC(10));
ads124s08->hw_tf->write_command(dev,ADS124S08_CMD_START );
k_sleep(K_MSEC(10));
ads124s08->hw_tf->write_command(dev,ADS124S08_CMD_STOP );
k_sleep(K_MSEC(10));
ads124s08->hw_tf->write_command(dev,ADS124S08_CMD_START );
#endif
return 0;
}
#if DT_NUM_INST_STATUS_OKAY(DT_DRV_COMPAT) == 0
#warning "ADS124S08 driver enabled without any devices"
#endif
/*
* Device creation macro, shared by ADS124S08_DEFINE_SPI() and
*/
#define ADS124S08_DEVICE_INIT(inst) \
DEVICE_DT_INST_DEFINE(inst, \
ads124s08_init, \
NULL, \
&ads124s08_data_##inst, \
&ads124s08_config_##inst, \
POST_KERNEL, \
CONFIG_SENSOR_INIT_PRIORITY, \
&ads124s08_driver_api);
#define IS_LSM303AGR_DEV(inst) \
DT_NODE_HAS_COMPAT(DT_DRV_INST(inst), st_lsm303agr_accel)
#define DISC_PULL_UP(inst) \
DT_INST_PROP(inst, disconnect_sdo_sa0_pull_up)
/*
* Instantiation macros used when a device is on a SPI bus.
*/
#define ADS124S08_HAS_CS(inst) DT_INST_SPI_DEV_HAS_CS_GPIOS(inst)
#define ADS124S08_DATA_SPI_CS(inst) \
{ .cs_ctrl = { \
.gpio_pin = DT_INST_SPI_DEV_CS_GPIOS_PIN(inst), \
.gpio_dt_flags = DT_INST_SPI_DEV_CS_GPIOS_FLAGS(inst), \
}, \
}
#define ADS124S08_DATA_SPI(inst) \
COND_CODE_1(ADS124S08_HAS_CS(inst), \
(ADS124S08_DATA_SPI_CS(inst)), \
({}))
#define ADS124S08_SPI_CS_PTR(inst) \
COND_CODE_1(ADS124S08_HAS_CS(inst), \
(&(ads124s08_data_##inst.cs_ctrl)), \
(NULL))
#define ADS124S08_SPI_CS_LABEL(inst) \
COND_CODE_1(ADS124S08_HAS_CS(inst), \
(DT_INST_SPI_DEV_CS_GPIOS_LABEL(inst)), (NULL))
#define ADS124S08_SPI_CFG(inst) \
(&(struct ads124s08_spi_cfg) { \
.spi_conf = { \
.frequency = \
DT_INST_PROP(inst, spi_max_frequency), \
.operation = (SPI_WORD_SET(8) | \
SPI_OP_MODE_MASTER | \
SPI_MODE_CPHA ), \
.slave = DT_INST_REG_ADDR(inst), \
.cs = ADS124S08_SPI_CS_PTR(inst), \
}, \
.cs_gpios_label = ADS124S08_SPI_CS_LABEL(inst), \
})
#ifdef CONFIG_ADS124S08_TRIGGER
#define GPIO_DT_SPEC_INST_GET_BY_IDX_COND(id, prop, idx) \
COND_CODE_1(DT_INST_PROP_HAS_IDX(id, prop, idx), \
(GPIO_DT_SPEC_INST_GET_BY_IDX(id, prop, idx)), \
({.port = NULL, .pin = 0, .dt_flags = 0}))
#else
#define ADS124S08_CFG_INT(inst)
#endif /* CONFIG_ADS124S08_TRIGGER */
#define ADS124S08_CONFIG_SPI(inst) \
{ \
.bus_name = DT_INST_BUS_LABEL(inst), \
.bus_init = ads124s08_spi_init, \
.bus_cfg = { .spi_cfg = ADS124S08_SPI_CFG(inst) }, \
ADS124S08_CFG_INT(inst) \
}
#define ADS124S08_DEFINE_SPI(inst) \
static struct ads124s08_data ads124s08_data_##inst = \
ADS124S08_DATA_SPI(inst); \
static const struct ads124s08_config ads124s08_config_##inst = \
ADS124S08_CONFIG_SPI(inst); \
ADS124S08_DEVICE_INIT(inst)
/*
* Main instantiation macro. Use of COND_CODE_1() selects the right
* bus-specific macro at preprocessor time.
*/
#define ADS124S08_DEFINE(inst) \
COND_CODE_1(DT_INST_ON_BUS(inst, spi), \
(ADS124S08_DEFINE_SPI(inst)), \
)
DT_INST_FOREACH_STATUS_OKAY(ADS124S08_DEFINE)
Ads124S08.h
#ifndef ZEPHYR_DRIVERS_SENSOR_ADS124S08_ADS124S08_H_
#define ZEPHYR_DRIVERS_SENSOR_ADS124S08_ADS124S08_H_
#include <kernel.h>
#include <device.h>
#include <sys/util.h>
#include <stdint.h>
#include <drivers/gpio.h>
#include <drivers/sensor.h>
#include <string.h>
#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
#include <drivers/spi.h>
#endif
#define DEBUG_MODE (1)
#if(DEBUG_MODE)
#define DEBUG_LOG LOG_INF
#else
#define DEBUG_LOG(...)
#endif
#define HIGH (0xFF)
#define LOW (0x00)
#define MULTI_CHANNEL_READ (0) // read through every channel
#define ENABLE_SOFT_CONFIGS (0)
#define HW_START (0) // Start through toggling START signal rater than sending start command
#define INTERNAL_TEMP_TEST (0)
#define MODE_CHANNEL_READ_ONLY (1) // Debug mode for reading channels, no internal measurment reading
#define PGA_GAIN_4
#define VREF (2.5)
// #define SINGLE_SHOT_MODE
#if defined(SINGLE_SHOT_MODE)
#define SINGLE_SHOT_MODE_BIT (0x20)
#else
#define SINGLE_SHOT_MODE_BIT (0x00)
#endif
// GPIO Pins
// #define ADS124S08_CS_LABEL DT_GPIO_LABEL(DT_ALIAS(gpiocus0), gpios)
// #define ADS124S08_CS_PIN DT_GPIO_PIN(DT_ALIAS(gpiocus0), gpios)
#define ADS124S08_RESET_LABEL DT_GPIO_LABEL(DT_ALIAS(gpiocus1), gpios)
#define ADS124S08_RESET_PIN DT_GPIO_PIN(DT_ALIAS(gpiocus1), gpios)
#define ADS124S08_START_LABEL DT_GPIO_LABEL(DT_ALIAS(gpiocus2), gpios)
#define ADS124S08_START_PIN DT_GPIO_PIN(DT_ALIAS(gpiocus2), gpios)
// Interrupt Pins
#if DT_INST_PROP_HAS_IDX(0, irq_gpios, 1)
/* INT1 is configured */
#define ADS124S08_INT1_GPIOS_PIN DT_INST_GPIO_PIN_BY_IDX(0, irq_gpios, 0)
#define ADS124S08_INT1_GPIOS_FLAGS DT_INST_GPIO_FLAGS_BY_IDX(0, irq_gpios, 0)
#define ADS124S08_INT1_GPIO_DEV_NAME DT_INST_GPIO_LABEL_BY_IDX(0, irq_gpios, 0)
#else
#define ADS124S08_INT1_GPIOS_PIN DT_INST_GPIO_PIN(0, irq_gpios)
#define ADS124S08_INT1_GPIOS_FLAGS DT_INST_GPIO_FLAGS(0, irq_gpios)
#define ADS124S08_INT1_GPIO_DEV_NAME DT_INST_GPIO_LABEL(0, irq_gpios)
#endif
#define DRDY_PIN (43)
#define RES (double)((double)VREF/pow(2,23))
// Commands
#define ADS124S08_CMD_NOP 0x00
#define ADS124S08_CMD_WAKEUP 0x02
#define ADS124S08_CMD_PWRDWN 0x04
#define ADS124S08_CMD_RESET 0x06
#define ADS124S08_CMD_START 0x08
#define ADS124S08_CMD_STOP 0x0A
#define ADS124S08_CMD_SYOCAL 0x16
#define ADS124S08_CMD_SYGCAL 0x17
#define ADS124S08_CMD_SFOCAL 0x19
#define ADS124S08_CMD_RDATA 0x12
#define ADS124S08_CMD_RREG 0x20
#define ADS124S08_CMD_WREG 0x40
#define RDATA_CMD_READ_BACK_LEN (3)
// Registers
#define ADS124S08_REG_ID 0x00
#define ADS124S08_REG_STATUS 0x01
#define ADS124S08_REG_INPMUX 0x02
#define ADS124S08_REG_PGA 0x03
#define ADS124S08_REG_DATARATE 0x04
#define ADS124S08_REG_REF 0x05
#define ADS124S08_REG_IDACMAG 0x06
#define ADS124S08_REG_IDACMUX 0x07
#define ADS124S08_REG_VBIAS 0x08
#define ADS124S08_REG_SYS 0x09
#define ADS124S08_REG_OFCAL0 0x0A
#define ADS124S08_REG_OFCAL1 0x0B
#define ADS124S08_REG_OFCAL2 0x0C
#define ADS124S08_REG_FSCAL0 0x0D
#define ADS124S08_REG_FSCAL1 0x0E
#define ADS124S08_REG_FSCAL2 0x0F
#define ADS124S08_REG_GPIODAT 0x10
#define ADS124S08_REG_GPIOCON 0x11
/* ADS124S0x common channels */
#define ADS124S08_AIN0 0x00
#define ADS124S08_AIN1 0x01
#define ADS124S08_AIN2 0x02
#define ADS124S08_AIN3 0x03
#define ADS124S08_AIN4 0x04
#define ADS124S08_AIN5 0x05
#define ADS124S08_AINCOM 0x0c
#define ADS124S08_AIN6 0x06
#define ADS124S08_AIN7 0x07
#define ADS124S08_AIN8 0x08
#define ADS124S08_AIN9 0x09
#define ADS124S08_AIN10 0x0a
#define ADS124S08_AIN11 0x0b
#define ADS124S08_MAX_CHANNELS 12
#define ADS124S08_POS_MUX_SHIFT 0x04
#define ADS124S08_INT_REF 0x09
#define ADS124S08_START_REG_MASK 0x1f
#define ADS124S08_NUM_BYTES_MASK 0x1f
#define ADS124S08_START_CONV 0x01
#define ADS124S08_STOP_CONV 0x00
#define ADS124S08_CHIP_ID 0x08
#if defined(PGA_GAIN_1)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_1
#define ADS124S08_PGA_FACTOR 1
#elif defined(PGA_GAIN_2)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_2
#define ADS124S08_PGA_FACTOR 2
#elif defined(PGA_GAIN_4)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_4
#define ADS124S08_PGA_FACTOR 4
#elif defined(PGA_GAIN_8)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_8
#define ADS124S08_PGA_FACTOR 8
#elif defined(PGA_GAIN_16)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_16
#define ADS124S08_PGA_FACTOR 16
#elif defined(PGA_GAIN_32)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_32
#define ADS124S08_PGA_FACTOR 32
#elif defined(PGA_GAIN_64)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_64
#define ADS124S08_PGA_FACTOR 64
#elif defined(PGA_GAIN_128)
#define ADS124S08_PGA_IDX ADS_PGA_GAIN_128
#define ADS124S08_PGA_FACTOR 128
#endif
#define ADS_PGA_GAIN_1 0x00
#define ADS_PGA_GAIN_2 0x01
#define ADS_PGA_GAIN_4 0x02
#define ADS_PGA_GAIN_8 0x03
#define ADS_PGA_GAIN_16 0x04
#define ADS_PGA_GAIN_32 0x05
#define ADS_PGA_GAIN_64 0x06
#define ADS_PGA_GAIN_128 0x07
#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
struct ads124s08_spi_cfg {
struct spi_config spi_conf;
const char *cs_gpios_label;
};
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */
union ads124s08_bus_cfg {
#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
const struct ads124s08_spi_cfg *spi_cfg;
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */
};
struct ads124s08_config {
const char *bus_name;
int (*bus_init)(const struct device *dev);
const union ads124s08_bus_cfg bus_cfg;
};
struct ads124s08_transfer_function {
int (*read_reg)(const struct device *dev, uint8_t reg_addr,
uint8_t *value);
int (*write_reg)(const struct device *dev, uint8_t reg_addr,
uint8_t value);
int (*read_samp)(const struct device *dev, uint8_t *value);
int (*write_command)(const struct device *dev, uint8_t value);
};
union asd124s08_sample{
uint8_t bytes[3];
uint32_t raw[1];
};
struct ads124s08_data {
const struct device *bus;
const struct ads124s08_transfer_function *hw_tf;
union asd124s08_sample sample;
uint8_t tempRecordings[18]; // 3 bytes per sample * 6 channels = 18 bytes
double cjv;
double chanV;
double tempCj;
double tempTC;
uint8_t internalTempSetBit;
uint32_t drdyPinStatus;
#ifdef CONFIG_ADS124S08_TRIGGER
const struct device *dev;
const struct device *gpio_int1;
struct gpio_callback gpio_int1_cb;
sensor_trigger_handler_t handler_drdy;
atomic_t trig_flags;
enum sensor_channel chan_drdy;
#if defined(CONFIG_ADS124S08_TRIGGER_OWN_THREAD)
K_KERNEL_STACK_MEMBER(thread_stack, CONFIG_ADS124S08_THREAD_STACK_SIZE);
struct k_thread thread;
struct k_sem gpio_sem;
#elif defined(CONFIG_ADS124S08_TRIGGER_GLOBAL_THREAD)
struct k_work work;
#endif
#endif /* CONFIG_ADS124S08_TRIGGER */
#if DT_ANY_INST_ON_BUS_STATUS_OKAY(spi)
struct spi_cs_control cs_ctrl;
#endif /* DT_ANY_INST_ON_BUS_STATUS_OKAY(spi) */
};
#ifdef CONFIG_ADS124S08_TRIGGER
int ads124s08_trigger_set(const struct device *dev,
const struct sensor_trigger *trig,
sensor_trigger_handler_t handler);
int ads124s08_init_interrupt(const struct device *dev);
#endif
int ads124s08_spi_init(const struct device *dev);
#endif
如有任何帮助,我们将不胜感激。
谢谢!
马特