This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1299:应用外部电压时通道电极上的输入电流。

Guru**** 2556980 points
Other Parts Discussed in Thread: ADS1299

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1100754/ads1299-input-current-on-channel-electrode-when-external-voltage-is-applied

部件号:ADS1299

我在概念上有疑问,如果ADS1299数据表显示PGA的输入阻抗为~1Gohm,并且它可以承受高达10mA的电流,这是否意味着通道输入引脚(InxP和InxN)可以提供高达1万V的电压?  

我在每个通道引脚上增加了2.2Kohm的保护电阻,并且电极引脚上有浪涌二极管,正如数据表所说的那样添加它。 当所有通道都提供7V的共模信号时,我尝试使用EEG信号(电阻= 6.5Kohm)。 我发现通道电极中的输入电流约为0.1mA。 如果InxP/InxN之后的运算放大器具有1Gohm直流输入阻抗,为什么0.1mA仍会进入它? 该电流也被发现进入偏置电极。 图示如下:

未显式设置ADS1299的所有寄存器。 当ADS1299启动时,它们为默认值,重置状态寄存器值。 意味着应禁用偏置放大器/缓冲器(如CONFIIG3=60h),但它仍然是沉降电流。 我在BIASOUT测量到的电压为+3V。 如果未应用外部共模电压,BIASOUT产生+2.5V (=AVDD)。 根据复位值中的CONFIIG3和BIANS_SENSP/SENSN,不应发生这种情况。  

ADS1299由VREFP和VREFN之间的双极电源AVDD=+2.5V,AVSS=-2.5V,VREFN = AVSS,VREFP=10uF电容器供电(数据表9.3 .1.3 .4)