This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS131M08:ADS131M08 EXT.Vref?

Guru**** 2826755 points

Other Parts Discussed in Thread: ADS131M08, ADS131E08

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1113607/ads131m08-ads131m08-ext-vref

器件型号:ADS131M08
主题中讨论的其他器件: ADS131E08

数据表中将 ADS131M08 EXT.REFIN MAX 描述为 AVDD + 0.3V、建议运行条件为1.1V ~ 1.3V。
如果使用2V 电压施加 REFIN、基准电压是否可以使用2V 电压运行? 还是在1.3V 下工作?
谢谢你。