This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DDC112:需要电源建议

Guru**** 2984610 points

Other Parts Discussed in Thread: DDC112, LM76005

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1058554/ddc112-need-suggestion-for-power-supply

器件型号:DDC112
主题中讨论的其他器件: LM76005
你好
为了获得最大的测量精度、我想选择一个低噪声线性稳压器来为 DDC112提供5V 电源。
线性稳压器的输入为来自直流/直流降压转换器 LM76005的12V。 最大电流要求小于300mA。
 
您能不能推荐任何合适的宽输入范围低噪声线性/LDO 稳压器为 DDC112提供精确的5V 电源?
或任何其他为 DDC112供电的解决方案以实现最大测量精度?