请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ADS7882 ADS7882外部基准输入的电压范围是多少? 例如、我可以在 ADC 上使用4.096V 或2.048V 基准、使输出直接对应十进制数、即0.001V 或0.0005V、还是必须使用2.56V 基准才能实现这一目的?
感谢您的任何帮助!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.