This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1299:ADS1299

Guru**** 2558250 points
Other Parts Discussed in Thread: ADS1299

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/786132/ads1299-ads1299

器件型号:ADS1299

我正在尝试将 Ads1299子板连接到 Arduino UNO。 但 DRDY 绝不会切换、SCK 不 会提供任何脉冲。

连接 方式如下:

通道1 -输入已给出

JP 6 -(1-2)已关闭

JP 7-(1-2)关闭

JP8- -(1-2)闭合

Jp5 -断电连接高电平  

Jp21 -(1-2)已关闭

Jp22 -(2-3)已关闭

JP23 -(1-2)已关闭

电源-中偏置(-2.5至2.5) AVDD - avss。

----------------------------------------------------

#include "pins_Arduino.h"
#include "ADS.h"

void setup(){

     Serial.begin(9600);
     serial.println ("ADS1299-bridge has started!");

ads_setup();
ads_reset ();
ADS_wreg (0x03、0xE0);       //CONFIG3 E0h 用于内部基准
ADS_wreg (0x01、0x96);       //config1 96h 默认值
ADS_wreg (0x02、0xC0);       //CONFIG2 C0h Deafault
ADS_wreg (0x05、0x01);       //将通道1设置为输入短路
ads_start();

void loop(){
ads_update_data();

------------------------

void ads_wreg (字符地址、字符值){

char opcode1 = 0x40 +地址;         //001rrrrrr;_rREG = 00100000且_address = rrrrrr
digitalWrite (cs、low);                 //低至已通信
SPI.transfer (0x11);                   //SDATAC
spi.transfer (optode1);                //RREG
SPI.transfer (0x00);
spi.transfer (value);
SPI.transfer (0x10);                 //重新打开连续读取数据
digitalWrite (cs、HIGH);               //高端通信

void ads_update_data(){
       if (digitalRead (DRDY)= low){
       serial.println ("ADS1299");
       digitalWrite (cs、low);
       SPI.transfer (0x10);
       长输出[9];
       长数据包;
       for (int i = 0;i<9;i++){
          for (int j = 0;j<3;j++){
            char dataByte = SPI.transfer (0x00);
            dataPacket =(dataPacket << 8)| dataByte;

output[i]= dataPacket;
dataPacket = 0;

digitalWrite (cs、HIGH);
serial.println (output[1]);           //仅打印通道1

输出:  

它始终读取为零