This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1299:为什么数据表中的直流导联脱落检测示例能够在 FDR/4下实现交流导联脱落检测?

Guru**** 2558250 points
Other Parts Discussed in Thread: ADS1299

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1172086/ads1299-why-does-datasheet-example-for-dc-lead-off-detection-enable-ac-lead-off-detection-at-fdr-4

器件型号:ADS1299

您好!

在最新(2017年1月修订) ADS1299数据表的第10.1.2.1节中、直流导联脱落示例建议将 LOFF 寄存器设置为0x13

这与寄存器说明相矛盾

位4:被保留并且应该一直为0

FLEAD_OFF[1:0]:对于直流导联脱落、这些位应为00

这是否是数据表中的错误?

如果是、那么对于启用直流导联脱落检测、将 导联脱落电流设置为6nA 并将比较器阈值设置为95%P 和5%N、LOFF 的正确值是否应为0x00?

Ankit