This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1605:关于 TUE 计算

Guru**** 2555630 points
Other Parts Discussed in Thread: ADS1605

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/612332/ads1605-about-tue-calculation

器件型号:ADS1605

你(们)好

以下 TUE 计算是正确的?

 

FSR (满量程范围)= 2 x 1.467 x Vref = 2 x 1.467 x (VREFP 引脚─VREFN 引脚)

               [ ADS1605는 Vref =最大3V 重命令]

                                    = 2 x 1.467 x 3V = 8.802V。 =>因此、ADC 输出代码将 为±4.401V

 

1 LSB = FSR/2^16 = 8.802V/65536 = 134.308 uV

 

偏移误差= 0.05[%FSR]= 0.05/100 x 8.802V = 4.401mV = 4.401mV/134.308uV =±32.77[LSB]

±误差漂移= 1 [ppmFSR/μ ⁰C = 1/10000 [%FSR/μ ⁰C = 1/10000 [%FSR/μ ⁰C x 65⁰C = 0.0065[%FSR]= 0.0065/100 x 8.802V = 0.57213mV= 0.57213mV/134.308uV = 4.26[LSB]。

               [  40⁰C - 25⁰C - 65⁰C |=、、]

   ±、在40⁰C~85⁰C μ V 的工作温度范围内、最大偏移为±μ V (4.401mV + 0.57213mV)= 4.973mV。

 

增益误差= 0.25[%]= 0.25/100 x 8.802V = 22.005mV = 22.005mV/134.308 UV =±163.84[LSB]

增益误差漂移= 10[ppm/μ ⁰C = 10/10000[%/μ ⁰C = 10/10000 x 65[%]= 0.065[%]= 0.065/100 x 8.802V = 5.721mV = 5.721mV/134.308uV =±42.60[LSB]

               [ 40⁰C - 25⁰C - 65⁰C |=、、]

 

INL =±0.75[LSB]

 

DNL =±0.25[LSB]

 

因此 、TUE = sqrt [(32.77+4.26)^2 +(164.84+42.6)^2 + 0.75^2 + 0.25^2]

                        = sqrt [37.03^2 + 207.44^2 + 0.75^2 + 0.25^2]

                        =±210.72[LSB]= 210.72[LSB] x 134.308uV =±28.3mV