This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE4400:信号强度

Guru**** 2974170 points

Other Parts Discussed in Thread: AFE4400

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/755829/afe4400-signal-strength

器件型号:AFE4400

使用 " Fluke ProSim Spot Light SpO2脉动式血氧计分析仪"校准我们的定制 AFE4400板。

afe4400 寄存器配置与 afe4400spo2_EVM 相同。 使用相同的配置(Led1、2 = 4mA)、 ProSim 上显示的信号强度约为30%。

因此,为了提高信号强度(60-70%),我们将 LED1、2电流从4mA 增加到10mA。 因此、红色和红外 ADC 数据饱和。

如何在保持良好信号强度的同时防止 ADC 饱和?

Fluke Spot Light 的建议信号强度是多少?