This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [常见问题解答] AFE5809:要支持声纳应用、需要在标准超声波设置中对 AFE5809进行哪些修改?

Guru**** 2927270 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/711628/faq-afe5809-to-support-sonar-applications-what-are-the-modifications-to-be-done-in-afe5809-from-the-standard-ultrasound-setup

器件型号:AFE5809

LNA 的直流失调电压校正电路由一个由 CBYPASS 设定的转角频率的 HPF 组成,该频率必须更改为1uF,以防止信号<100kHz 时的输入信号衰减。

http://e2e.ti.com/support/applications/medical/f/30/t/549672

http://www.ti.com/lit/ug/tidu702/tidu702.pdf