Other Parts Discussed in Thread: TLV5632
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV5632 您好、请告诉我。
对于 TLV 5632、REF 端子为 I/O.请告诉我如何将其用作输入引脚。
如果 REF 端子连接到+5V 且 AGND·DGND 连接到 GND、模拟输出电压的满量程是否会从5V 变为0V?
此致、
O安全。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.