请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ADS1118 你(们)好
我正在使用 ATMEGA32A 和 ADS1118从事1000度的熔炉控制器工作。 我从 github.com/hydrosense 下载了 ads1118库。当我单独读取环境温度或热电偶时、一切都正常、但当我想同时读取这两者时、数字会相等。 我的意思是环境温度和热电偶显示相同的数字(内部传感器值)。 如果有人能提供帮助,将不胜感激。
此致
#include
#include
#include
#include "Ads1118.h"
#include
CONST int LS100_LED = 8;
CONST int LS200_LED = 9;
CONST int Metalcast_LED = 10;
CONST int HP_LED = 11;
CONST int MP_LED = 12;
CONST int LP_LED = 13;
CONST int LS100_SW = 24;
CONST int LS200_SW = 25;
CONST = 26 INT_SW
;CONST = 27;CONST = INT_SW;CONST = INT_SW;CONST = INT_SW
const int MP_SW = 28;
const int LP_SW = 30;
const int start_SW = 29;
const int stop_SW = 31;
const int SSR = 3;
const int 继电器= 4;
const int 蜂鸣器= 2;
//const int TEMP = 1;//ADS1232/const
int MUX = 0; //ADS1232
//const int GAIN0 = 23;//ADS1232
//const int GAIN1 = 22;//ADS1232
//const int speed = 21;//ADS1232
//const int PWDN = 20;//ADS1232//const
int SCLK = 15;//ADS1232 /const
int 缓冲区= 10;/dprom = 0.90;/int float = 10;/dm = d.int EEPROM
unsigned long lastmillis1 = 0;
unsigned long lastmillis2 = 0;
unsigned long lastmillis3 = 0;
unsigned long lastmillis4 = 0;
float Ctemp = 0;
// int Eraser = 0b10000000;
// int Prescaler = 0b01101010;
LiquidCrystal _I2C LCD (0x27、2、1、0、0、0、 4、5、6、7、3、 正极);// I2C 地址可以是0x3F 或0x27
Ads1118 ads1118 (1);
void setup ()
{
pinMode (LS100_LED、输出);
pinMode (LS200_LED、输出);
pinMode (Metalcast_LED、 输出);
pinMode (HP_LED、输出);
pinMode (MP_LED、输出);
引脚模式(LP_LED、输出);
引脚模式(LS100_SW、INPULLUP);
引脚模式(LS200_SW、 Input_pullup);
pinMode (Metalcast_SW、input_pullup);
pinMode (HP_SW、input_pullup);
引脚模式(MP_SW、INPUT_PULLUP);
引脚模式(LP_SW、INPULLUP);
引脚模式(START_SW、 INPUT_PULLUP);
引脚模式(STOP_SW、INPULLUP);
引脚模式(蜂鸣器、输出);;
pinMode (继电器、输出);
pinMode (SSR、输出);
// pinMode (TEMP、 输出);//ADS1232
// pinMode (MUX、输出);//ADS1232
// pinMode (GAIN0、输出); //ADS1232
// pinMode (GAIN1、OUTPUT);//ADS1232
// pinMode (SPEED、OUTPUT);//ADS1232
// pinMode (PWDN、 输出);//ADS1232
// pinMode (SCLK、输出);//ADS1232
// pinMode (DRDY、输入); //ADS1232
// digitalWrite (TEMP、LOW);
// digitalWrite (MUX、LOW);
// digitalWrite (GAIN0、 高电平);
// digitalWrite (GAIN1、高电平);
// digitalWrite (speed、高电平);
// digitalWrite (PWDN,高电平);
Wire.begin();
delay (500);
digitalWrite (SSR, low );
digitalWrite( relay, low );
lcd.begin(16,2);
lcd.clear();
ads1118.begin();
ads1118.setGain(0b101);
///========================= PWM 频率预分频器===================
//TCCR2 &=橡皮擦;
// TCCR2 |=预分频器;
// ocr2 = 0x00;
////========================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================================
lcd.setCursor(0、0);
lcd.print (" LIDOMA Ltd ");
lcd.setCursor(0、1);
lcd.print (" Pressmatik ");
delay (3000);
lcd.setCursor(0、0);
lcd.print ("选择程序");
lcd.setCursor(0、1);
lcd.print (") ");
}
void loop(){
if ( digitalRead ( LS100_SW )== low ){
digitalWrite (LS100_LED,高电平);
digitalWrite (LS200_LED,低电平);
digitalWrite (Metalcast_LED,low);
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,low);
digitalWrite (hp_LED,low);
Buffer = 10;
lcd.clear();
lcd.setCursor(0、0);
lcd.print (" 100克 ");
//Display();
}
如果( digitalRead ( LS200_SW )=low ){
digitalWrite (LS100_LED,低电平);
digitalWrite (LS200_LED,高电平);
digitalWrite (Metalcast_LED,low);
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,low);
digitalWrite (hp_LED,low);
Buffer = 20;
lcd.clear();
lcd.setCursor(0、0);
lcd.print (" 200克 ");
//Display();
}
如果(digitalRead (Metalcast_SW)== low)则为{
digitalWrite (LS100_LED,低电平);
digitalWrite (LS200_LED,低电平);
digitalWrite (Metalcast_LED,高电平);
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,low);
digitalWrite (hp_LED,low);
缓冲区= 30;
lcd.clear();
lcd.setCursor(0、0);
lcd.print (" pfm preheat ");
//Display();
}
否则,如果(( digitalRead ( LP_SW )== low )&&( Buffer=10|| Buffer=12 )){
digitalWrite (LP_LED,高电平);
digitalWrite (MP_LED,low);
digitalWrite (hp_LED,low);
Buffer = 11;
Htemp = 910;
//lcd.clear();
lcd.setCursor(0、1);
lcd.print ("HT-MT-HO-Impulim");
//Display();
}
否则,如果(( digitalRead ( MP_SW )== low )&&( Buffer=10|| Buffer=11 )){
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,高电平);
digitalWrite (hp_LED,low);
缓冲区= 12;
Htemp = 915;
//lcd.clear();
lcd.setCursor(0、1);
lcd.print (" LT-MO ");
//Display();
}
否则,如果(( digitalRead ( LP_SW )== low )&&( Buffer == 20 || Buffer == 22 || Buffer == 23 )){
digitalWrite (LP_LED,高电平);
digitalWrite (MP_LED,low);
digitalWrite (hp_LED,low);
缓冲区= 21;
Htemp = 915;
//lcd.clear();
lcd.setCursor(0、1);
lcd.print ("HT-MT-HO-Impulim");
//Display();
}
否则,如果(( digitalRead ( MP_SW )== low )&&( Buffer == 20 || Buffer == 21 || Buffer == 23 )){
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,高电平);
digitalWrite (hp_LED,low);
Buffer = 22;
Htemp = 917;
//lcd.clear();
lcd.setCursor(0、1);
lcd.print (" 左 ");
//Display();
}
否则,如果(( digitalRead ( HP_SW )=low )&&( Buffer==20|| Buffer=21|| Buffer==22 )){
digitalWrite (LP_LED,低电平);
digitalWrite (MP_LED,low);
digitalWrite (HP_LED,高电平);
缓冲区= 23;
Htemp = 920;
//lcd.clear();
lcd.setCursor(0、1);
lcd.print (" 穆 ");
//Display();
}
如果(digitalRead (start_SW)== low)则为{
STARTPRESS ();
}
//delay (50);
float A =(ads1118.adsReadRaw (ads1118.DIF01)* 0.256 / 32768)* 1000;
//float B = ads1118.readTemp ();
lcd.setCursor(0、0);
lcd.print (" ");
//lcd.print( B,1 );
lcd.print(" ");
lcd.setCursor(0,1);
lcd.print(" ");
lcd.print( convert (A),5);
lcd.print(" ");
//ads1118.update_config (0x008B);
delay (50);
}
void STARTPRESS (){
float translat (float MV){
float T = 137.9263 +(((((MV - 0.93395)*(0.09615 * MV * MV * MV * MV * MV * MV * MV + 19.62905 * MV * MV * MV * MV * MV + 73.97377 *)*)/ 1.330451) (0.20813 * MV * MV + 0.57668 * MV + 0.27986));
///float T = 137.92 +(127.61*(MV - 0.933)+ 110.89*(MV - 0.965)*(MV - 0.933)+ 19.89*(MV - 0.933)*(MV - 0.933)*(MV - 0.933)*(MV )+ 0.096*(MV - 0.965)*(MV - 0.933)*(MV )*(SV - 0.933*(SV - 0.933)*(SV - 0.933)*(SV - 0.933*(SV - 0.933)*(SV - 0.933)*(SV - 0.933*(SV - 0.933)*(SV - 0.933*(SV -
0.