This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADC3683:连接器件时钟

Guru**** 2943430 points

Other Parts Discussed in Thread: ADC3682, ADC3681, ADC3683

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1225644/adc3683-connecting-device-clock

器件型号:ADC3683
主题中讨论的其他器件:ADC3681、ADC3682、

您好!

数据表说明输入时钟频率的工作范围为0.5MHz 至65MHz。

它与65MSPS 的采样率有何关系?

是这样吗?

  • ADC3681:10MSPS -> 10MHz
  • ADC3682:25MSPS --> 25MHz
  • ADC3683:65MSPS -> 65MHz

感谢您的帮助。