This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1278-SP:如果在初始上电期间短暂违反电压限制、这是否会影响器件的可靠性?

Guru**** 2553450 points
Other Parts Discussed in Thread: ADS1278

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1412234/ads1278-sp-if-voltage-constrains-are-violated-briefly-during-intial-power-up-will-that-affect-the-part-s-reliability

器件型号:ADS1278-SP
主题中讨论的其他器件:ADS1278

工具与软件:

如果 AINP1 - AINP8模拟输入在上电期间出现瞬变、超过 AVDD 当前所在位置(或比 AGND 低0.1V) 0.1V 以上、从而违反数据表的限制、这是否会影响器件的可靠性? 例如、假设 AINP1在初始上电期间快速降至-1V 并持续50ms、在这50ms 期间、AVDD 仍为零、这是否会导致长期可靠性问题?