This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE4403:驱动高电压 LED

Guru**** 2912410 points

Other Parts Discussed in Thread: AFE4403

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1449192/afe4403-to-drive-high-voltage-led

器件型号:AFE4403

工具与软件:

大家好、我想使用 AFE4403在共阳极模式下驱动 UV LED、LED 所需电压为5-7V、因为最大电压是5.25-0.5=4.75V?
是否可能驱动此 UV LED

如果4403无法直接提供高电压、是否有其他方法可以提供额外的高电压、以便我可以使用4403  同时控制 UV LED 和其他 LED?

此外、如果 LED 反向并用作 PD、驱动电压是否也需要达到7V 才能读取信号?

此致